public static class AdvancedFlangeBuilder.LengthReferences extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIN6935 |
static int |
_INSIDE |
static int |
_OUTSIDE |
static int |
_WEB |
static AdvancedFlangeBuilder.LengthReferences |
DIN6935 |
static AdvancedFlangeBuilder.LengthReferences |
INSIDE |
static AdvancedFlangeBuilder.LengthReferences |
OUTSIDE |
static AdvancedFlangeBuilder.LengthReferences |
WEB |
Modifier and Type | Method and Description |
---|---|
static AdvancedFlangeBuilder.LengthReferences |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AdvancedFlangeBuilder.LengthReferences |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AdvancedFlangeBuilder.LengthReferences[] |
values()
Returns an array that contains the values for this enum.
|
public static final AdvancedFlangeBuilder.LengthReferences INSIDE
public static final AdvancedFlangeBuilder.LengthReferences OUTSIDE
public static final AdvancedFlangeBuilder.LengthReferences WEB
public static final AdvancedFlangeBuilder.LengthReferences DIN6935
public static final int _INSIDE
public static final int _OUTSIDE
public static final int _WEB
public static final int _DIN6935
public static AdvancedFlangeBuilder.LengthReferences valueOf(int value)
public static AdvancedFlangeBuilder.LengthReferences valueOf(String name)
public static AdvancedFlangeBuilder.LengthReferences[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.