Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static ContourFlangeBuilder.SectionSideOptions |
ContourFlangeBuilder.SectionSideOptions.LEFT |
static ContourFlangeBuilder.SectionSideOptions |
ContourFlangeBuilder.SectionSideOptions.RIGHT |
Modifier and Type | Method and Description |
---|---|
ContourFlangeBuilder.SectionSideOptions |
ContourFlangeBuilder.thicknessSide()
Returns the thickness side of contour flange
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static ContourFlangeBuilder.SectionSideOptions |
ContourFlangeBuilder.SectionSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContourFlangeBuilder.SectionSideOptions |
ContourFlangeBuilder.SectionSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContourFlangeBuilder.SectionSideOptions[] |
ContourFlangeBuilder.SectionSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ContourFlangeBuilder.setThicknessSide(ContourFlangeBuilder.SectionSideOptions sectionSide)
Sets the thickness side of contour flange
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.