Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static ClosedCornerBuilder.ClosureTypeOptions |
ClosedCornerBuilder.ClosureTypeOptions.CLOSE |
static ClosedCornerBuilder.ClosureTypeOptions |
ClosedCornerBuilder.ClosureTypeOptions.OVERLAP |
Modifier and Type | Method and Description |
---|---|
ClosedCornerBuilder.ClosureTypeOptions |
ClosedCornerBuilder.closureType()
Returns the closure type
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
static ClosedCornerBuilder.ClosureTypeOptions |
ClosedCornerBuilder.ClosureTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ClosedCornerBuilder.ClosureTypeOptions |
ClosedCornerBuilder.ClosureTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ClosedCornerBuilder.ClosureTypeOptions[] |
ClosedCornerBuilder.ClosureTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ClosedCornerBuilder.setClosureType(ClosedCornerBuilder.ClosureTypeOptions closureType)
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.