Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static LouverBuilder.EndTypeOptions |
LouverBuilder.EndTypeOptions.FORMED |
static LouverBuilder.EndTypeOptions |
LouverBuilder.EndTypeOptions.LANCED |
Modifier and Type | Method and Description |
---|---|
LouverBuilder.EndTypeOptions |
LouverBuilder.endType()
Returns the end type for the louver.
|
static LouverBuilder.EndTypeOptions |
LouverBuilder.EndTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LouverBuilder.EndTypeOptions |
LouverBuilder.EndTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LouverBuilder.EndTypeOptions[] |
LouverBuilder.EndTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LouverBuilder.setEndType(LouverBuilder.EndTypeOptions endType)
Sets the end type for the louver.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.