Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BeadBuilder.HeightSideOptions |
BeadBuilder.HeightSideOptions.SECTION_NORMAL_SIDE
Material removed on the side of the section normal.
|
static BeadBuilder.HeightSideOptions |
BeadBuilder.HeightSideOptions.SECTION_REVERSE_NORMAL_SIDE
Material removed on the side opposite to that of the section normal
|
Modifier and Type | Method and Description |
---|---|
BeadBuilder.HeightSideOptions |
BeadBuilder.heightSide()
Returns the Height side for the bead.
|
static BeadBuilder.HeightSideOptions |
BeadBuilder.HeightSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BeadBuilder.HeightSideOptions |
BeadBuilder.HeightSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BeadBuilder.HeightSideOptions[] |
BeadBuilder.HeightSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BeadBuilder.setHeightSide(BeadBuilder.HeightSideOptions heightSide)
Sets the Height side for the bead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.