Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Method and Description |
---|---|
BendListItemBuilder |
SheetmetalManager.createBendListItemBuilder()
Creates a
BendListItemBuilder
BendListItemBuilder objects will be created and populated in the BendListBuilder when bend information of a flat pattern view is populated. |
BendListItemBuilder |
BendListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
BendListItemBuilder[] |
BendListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BendListItemBuilderList.append(BendListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
BendListItemBuilderList.append(BendListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BendListItemBuilderList.erase(BendListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
BendListItemBuilderList.erase(BendListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BendListItemBuilderList.findIndex(BendListItemBuilder obj)
Finds the index where the input object appears.
|
void |
BendListItemBuilderList.insert(int location,
BendListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
BendListItemBuilderList.setContents(BendListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
BendListItemBuilderList.swap(BendListItemBuilder object1,
BendListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.