Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static BendTaperBuilder.BendTaperType |
BendTaperBuilder.BendTaperType.LINEAR
Linear
|
static BendTaperBuilder.BendTaperType |
BendTaperBuilder.BendTaperType.SQUARE
Square
|
static BendTaperBuilder.BendTaperType |
BendTaperBuilder.BendTaperType.TANGENT
Tangent
|
Modifier and Type | Method and Description |
---|---|
BendTaperBuilder.BendTaperType |
BendTaperBuilder.bendTaperType1()
Returns the bend taper type for Side 1
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
BendTaperBuilder.BendTaperType |
BendTaperBuilder.bendTaperType2()
Returns the bend taper type for Side 2
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
static BendTaperBuilder.BendTaperType |
BendTaperBuilder.BendTaperType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendTaperBuilder.BendTaperType |
BendTaperBuilder.BendTaperType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendTaperBuilder.BendTaperType[] |
BendTaperBuilder.BendTaperType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendTaperBuilder.setBendTaperType1(BendTaperBuilder.BendTaperType bendTaperType1)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
void |
BendTaperBuilder.setBendTaperType2(BendTaperBuilder.BendTaperType bendTaperType2)
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.