Package | Description |
---|---|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
Modifier and Type | Field and Description |
---|---|
static JogBuilder.DimensionTypeOptions |
JogBuilder.DimensionTypeOptions.FULL
the actual extent distance will be the value specified as depth.
|
static JogBuilder.DimensionTypeOptions |
JogBuilder.DimensionTypeOptions.OFFSET
the actual depth will be depth plus the thickness of sheet.
|
Modifier and Type | Method and Description |
---|---|
JogBuilder.DimensionTypeOptions |
JogBuilder.dimensionType()
Returns the Offset Dimension
The actual extent distance of the Jog will be determined by the active dimension option. |
static JogBuilder.DimensionTypeOptions |
JogBuilder.DimensionTypeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JogBuilder.DimensionTypeOptions |
JogBuilder.DimensionTypeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JogBuilder.DimensionTypeOptions[] |
JogBuilder.DimensionTypeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JogBuilder.setDimensionType(JogBuilder.DimensionTypeOptions dimensionType)
Sets the Offset Dimension
The actual extent distance of the Jog will be determined by the active dimension option. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.