Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Class and Description |
---|
AddReusablePartCollection
Represents a collection of AddReusablePart
To obtain an instance of this class, refer to Part Created in NX5.0.0 |
CAMDataManager
Represents an object that manages cam data objects.
|
ToolingManager
Contains the collection objects for creating and iterating over Reuse Library objects.
|
ToolingSession |
Class and Description |
---|
CaeReuseLibrary
Represents a
CaeReuseLibrary
To obtain an instance of this class, refer to BaseFEModel Created in NX7.5.2 |
Class and Description |
---|
PrebendBuilder
Represents a
PrebendBuilder builder to divide bend faces. |
UniversalUnformBuilder
Represents a
UniversalUnformBuilder builder. |
Class and Description |
---|
AddReusableFeatureCollection
Represents a collection of AddReusableFeature
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
AddReusableFeatureCollection.InputData
Defines the input data of AddReusableFeatureBuilder
|
AddReusablePart
Represents a
AddReusablePart
To create a new instance of this class, use AddReusablePartCollection.createBuilder() Created in NX5.0.0 |
AddReusablePart.ModeMethod
Represents adding or editing a reusable component mode method
|
AddReusablePart.PositionMethod
Represents the position method
|
AssemblyDrawingBuilder
Represents a
AssemblyDrawingBuilder which is
used to create or edit the Assembly Drawing. |
AssemblyDrawingBuilder.AttributeNames
Specifies the attribute name
|
AssemblyDrawingBuilder.AttributeValues
Specifies the attribute value.
|
AssemblyDrawingBuilder.DrawingCreateOrEdit
Specifies the sheet operation.
|
AssemblyDrawingBuilder.DrawingTypes
Specifies the drawing type.
|
AssemblyDrawingBuilder.ModelViewToUseValue
Specifies the model view to use.
|
AssemblyDrawingBuilder.Types
Specifies the filter of assembly.
|
AssemblyDrawingBuilder.ViewOptionValue
Specifies the view options.
|
AssignPatchBuilder
Represents a builder to be used to add sheet bodies as patch surfaces or delete patch surfaces.
|
AssignPatchBuilder.PatchColorData
This class holds the data returned from
AssignPatchBuilder.getPatchColor() |
AssignPatchCollection
Represents a collection of AssignPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
AutoDieCollection
Represents a collection of Die Design Draw Punch
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
AutoDimensionBuilder
Represents a
AutoDimensionBuilder which is
used to create or edit the Auto Dimension. |
AutoDimensionBuilder.MainType
create or edit ordinate dimension
|
AutoDimensionBuilder.TextFontType
text font type
|
AutoDimensionBuilder.TextOrientationType
text orientation type
|
AutoDimensionBuilder.ToleranceType
tolerance type
|
AutoDimensionBuilder.ValuePrecisionType
value precision type
|
BackingPadBuilder
Represents a
BackingPadBuilder which is used to create or delete the Backing Pad. |
BackingPadBuilder.Types
types of backing pad design
|
BendInsertDesignBuilder
Represents a
BendInsertDesignBuilder
Bend Insert Design is to create inset puch or die for bend . |
BendInsertDesignBuilder.BendingDirectionOption
the bending direction.
|
BendInsertDesignBuilder.BendTypeOption
the bend type.
|
BendInsertDesignBuilder.BlankPositions
Specifies the blank position.
|
BendInsertDesignBuilder.InsertTypeOption
the insert type.
|
BendInsertDesignBuilder.ParentOption
the parent node.
|
BendInsertDesignBuilder.Types
the bending operation.
|
BendInsertDesignCollection
Creates a
BendInsertDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BendOperationBuilder
Represents a
BendOperationBuilder builder. |
BendOperationBuilder.OverbendOptions
The overbend option.
|
BendOperationBuilder.Prebend
The number of children bends of prebend.
|
BendOperationBuilder.Types
unbend operations.
|
BendOperationCollection
Creates a
BendOperationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlankGeneratorBuilder
Represents a
BlankGeneratorBuilder
This class is for Blank Generator Design UI
To create a new instance of this class, use BlankGeneratorCollection.createBlankGeneratorBuilder() Created in NX7.5.0 |
BlankGeneratorBuilder.CreateBlankType
Specify the creation method.
|
BlankGeneratorBuilder.EditBlankType
Specify the edit method.
|
BlankGeneratorBuilder.Types
Specifies the option of blank generator operation type.
|
BlankGeneratorCollection
Creates a
BlankGeneratorBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BlankLayoutBuilder
Progressive Die Wizard blank layout builder
To create a new instance of this class, use BlankLayoutCollection.createBlankLayoutBuilder() Default values. |
BlankLayoutBuilder.LeftRightSideOption
Specifies the option of left right side type.
|
BlankLayoutBuilder.SideWebOption
Specifies the option of side webs type.
|
BlankLayoutBuilder.SnapSizeOption
Specifies the option of snap size.
|
BlankLayoutBuilder.Types
Specifies the option of blank layout type.
|
BlankLayoutCollection
Creates a
BlankLayoutBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
BlankNestingBuilder
Blank Nesting Builder of PDW, EDW and Die Engineering.
|
BlankNestingBuilder.LayoutTypeSpecification
Specifies the layout type of blank nesting.
|
BlankNestingCollection
Creates a
BlankNestingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlendCurve3DBuilder
Represents a
BlendCurve3DBuilder builder which implements
blend curves in one side where the corner radius is too small. |
BlendCurve3DBuilder.BlendCurveOptions
The blend curve creation methods: Best Fit, Variable, Vector, Current View
|
BlendCurve3DBuilder.InputCurvesOption
The input curves option to keep, hide or delete input curves
|
BomBuilder
Represents a Tooling::BomBuilder builder
To create a new instance of this class, use BomCollection.createBomBuilder() Default values. |
BomBuilder.Circle
Represents an index to the base circle type of cylinder shape.
|
BomBuilder.Shape
Represents an index to the shape of stock size.
|
BomBuilder.TreeList
Represents an index to components list type.
|
BomCollection
Represents a collection of Bom
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
BomListBuilder
Represents a
BomListBuilder builder. |
BomListBuilder.BomListTypes
Represents an index to components list type.
|
BurringInsertBuilder
Progressive Die Wizard builder to design burring punch and die insert
To create a new instance of this class, use BurringInsertCollection.createBurringInsertBuilder() Default values. |
BurringInsertBuilder.BurringDirections
Specifies the burring direction.
|
BurringInsertBuilder.BurringPunchTypes
Specifies the burring punch type.
|
BurringInsertBuilder.CircularOrNonCircularType
Specifies the circular or non-circular type.
|
BurringInsertBuilder.DesignOptions
Specifies the design type.
|
BurringInsertBuilder.ParentTypes
Specifies the parent part type.
|
BurringInsertCollection
Creates a
BurringInsertCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CalculateAreaBuilder
The CalculateArea builder
To create a new instance of this class, use CalculateAreaCollection.createBuilder() Default values. |
CalculateAreaCollection
Represents a collection of CalculateArea builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ChangeoverManagementBuilder
Represents a
ChangeoverManagementBuilder to support changeover workflow management. |
ChangeoverManagementBuilder.Types
Specifies the types of changeover management.
|
ChannelAdjustBuilder
The builder class for Channel Adjust which assists you
to adjust the postion and the length of the channel.
|
ChannelAdjustBuilder.AdjustType
the adjust method.
|
ChannelAdjustBuilder.VectorMethod
the vector adjust method.
|
ChannelAdjustCollection
Creates a ChannelAdjust Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ChannelFittingBuilder
The builder class for Channel Fitting which assists you
to add cooling fitting.
|
ChannelFittingCollection
Creates a ChannelFitting Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ClearanceManagementBuilder
Progressive Die Wizard builder to management clearances.
|
ClearanceManagementBuilder.Selection
Specifies clearance management part.
|
ClearanceManagementBuilder.Type
Specifies type to assign or check clearances
|
ClearanceManagementCollection
Creates a
ClearanceManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CloneObject
Represents the clone operation in Add Reusable Component Builder.
|
ClonePart
Represents the part inforamtion to be cloned in Add Reusable Component Builder.
|
CompDrawingBuilder
Represents a
CompDrawingBuilder which is
used to create or edit the Component Drawing. |
CompDrawingBuilder.ComponentTypeSelection
Specifies the type of components.
|
CompDrawingBuilder.DrawingType
Specifies the drawing type.
|
CompDrawingBuilder.FilterSelection
Specifies the filter of components.
|
CompDrawingBuilder.ProjectionType
Specifies the project type.
|
ConceptPositionBuilder
concept position builder for standard part design
To create a new instance of this class, use ConceptPositionCollection.createConceptPositionBuilder() Created in NX6.0.0 |
ConceptPositionCollection
Represents a collection of ConceptPosition
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ConcurrentDesignManagementBuilder
Represents a
ConcurrentDesignManagementBuilder to support concurrent design workflow management. |
ConcurrentDesignManagementBuilder.Types
Specifies the types of concurrent design management.
|
ConcurrentDesignManagementBuilder.UpdateTypes
Specifies the types of the update action.
|
CoolingConnectBuilder
The builder class for Cooling connection which assists you
to create channel and connect it to other channels.
|
CoolingConnectCollection
Creates a CoolingConnect Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingDefineChannelBuilder
The builder class for Cooling Define Channel which assists you
to create channels directly.
|
CoolingDefineChannelBuilder.ExtensionTypes
The extension types of channel
|
CoolingDefineChannelBuilder.TipEndTypes
The tip end types of channel
|
CoolingDefineChannelBuilder.Types
Types to specify how to assign attributes to the created body.
|
CoolingDefineChannelCollection
Creates a CoolingDefineChannel Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingExtendBuilder
The builder class for Channel Extend which assists you
to extend the channel.
|
CoolingExtendBuilder.TipEndTypes
The tip end types of channel
|
CoolingExtendCollection
Creates a CoolingExtend Collection.
|
CoolingFittingData
Represents the cooling fitting data in Add Channel Fitting Builder.
|
CoolingPatternBuilder
The builder class for Cooling pattern which assists you
to create channels with selected curves.
|
CoolingPatternCollection
Creates a CoolingPattern Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CornerDesignBuilder
Represents a
CornerDesignBuilder ,
Corner Design is to provide tools to make corner. |
CornerDesignBuilder.CornerTypeOpt
the corner types
|
CornerDesignBuilder.SelectFromOpt
the object selection options.
|
CornerDesignBuilder.Types
The corner design type.
|
CornerDesignCollection
Creates a
CornerDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CreateBoxBuilder
Represents a box creation operation
To create a new instance of this class, use CreateBoxCollection.createBoxBuilder(nxopen.NXObject) Default values. |
CreateBoxBuilder.BoxType
the type for creating box
|
CreateBoxCollection
Creates CreateBoxBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DefineCamBuilder
Represents a
DefineCamBuilder to create different types of cam objects, which
are used for kinematic motion To create a new instance of this class, use ProgressiveDieManager.createDefineCamBuilder() Default values. |
DefineCamBuilder.Types
Specifies the cam types
|
DefineLifterBuilder
Represents a
DefineLifterBuilder to create different types of lifter objects, which
are used for kinematic motion. |
DefineLifterBuilder.Types
Specifies the lifter types
|
DefineNeutralFactorBuilder
Represeents a
DefineNeutralFactorBuilder to define
neutral factor according to material and formula in the spreadsheet table. |
DefineNeutralFactorBuilder.FormulaOptions
Specifies the formula used to calculate the neutral factor value
|
DesignTrimToolBuilder
Represents a builder to be used to create Mold Wizard design trim tool.
|
DesignTrimToolCollection
Creates a DesignTrimToolCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
DieBaseBuilder
Represents Progressive Die Wizard and Engineering Die Wizard builder to manage die base.
|
DieBaseBuilder.AlongDirectionOpt
along direction options.
|
DieBaseBuilder.CatalogOpt
catalog options.
|
DieBaseBuilder.DesignToolOption
design tool options.
|
DieBaseBuilder.DieBaseTypeOpt
die bse types options.
|
DieBaseBuilder.ParentNodeOpt
parent node options.
|
DieBaseBuilder.PlatesNumberOpt
plates number options.
|
DieBaseBuilder.SplitMethod
split method.
|
DieBaseBuilder.Types
die base types.
|
DieBaseCollection
Creates a
DieBaseCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DieDesDrawDieBuilder
Represents the Die Design draw die management builder, which is to create a draw die by selected
sheet body, curve and base plane.
|
DieDesDrawPunchBuilder
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve
and base plane.
|
DieDesignLowerBinderBuilder
Represents a Lower Binder builder
To create a new instance of this class, use AutoDieCollection.createDieDesignLowerBinderBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesignSettingBuilder
Represents a
DieDesignSettingBuilder
This class is for Die Design Setting UI
To create a new instance of this class, use DieDesignSettingCollection.createDieDesignSettingBuilder() Created in NX7.5.0 |
DieDesignSettingCollection
Creates a
DieDesignSettingBuilder . |
DieDesignTrimPostBuilder
Represents a Trim Post builder
To create a new instance of this class, use AutoDieCollection.createDieDesignTrimPostBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesPierceInsertBuilder
Represents Die Design Pierce Insert builder.
|
DieDesPierceInsertBuilder.Direction
Represents the thickness direction.
|
DieDesPierceInsertBuilder.HoleShapeTypes
Represents the hole shape type.
|
DieEngFormTaskBuilder
Represents a Form Task builder
To create a new instance of this class, use AutoDieCollection.createDieEngFormTaskBuilder(nxopen.features.Feature) Default values. |
DieEngProcessUpdateManagerBuilder
Die Engineer process update manager management builder.
|
DieEngProcessUpdateManagerBuilder.Types
the trim task or pierce task.
|
DieEngStampingCarryoverBuilder
Represents a Stamping Carryover builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingCarryoverBuilder(nxopen.features.BodyFeature) Created in NX10.0.0 |
DieEngStampingOutputBuilder
Represents a Stamping Output builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingOutputBuilder(nxopen.features.BodyFeature) Default values. |
DieEngStampingOutputBuilder.DisplayProductType
Types of product display.
|
DieEngStampingOutputBuilder.SpringbackMethodType
Types of springback method
|
DieEngTrimAngleCheckBuilder
Represents a Trim Angle Check builder
To create a new instance of this class, use AutoDieCollection.createDieEngTrimAngleCheckBuilder(nxopen.geometricanalysis.AnalysisObject) Default values. |
DieEngTrimAngleCheckBuilder.DirectionOptions
Options to determine the method to specify direction.
|
DieEngTrimTaskBuilder
Die Engineer trim task management builder, create a trim task by selected die tip, trim bounds,
start plane and end plane.
|
DieEngTrimTaskBuilder.TrimTaskCamType
the trim task cam type.
|
DieEngTrimTaskBuilder.TrimTaskMatchCutType
the trim task match cut type.
|
DirectUnbendBuilder
The builder contains all inputs for direct unbend.
|
DirectUnbendBuilder.Bendtypes
unbend operations.
|
DirectUnfoldBuilder
The builder contains all inputs for direct unfolding.
|
DirectUnfoldBuilder.Bend
The number of children bends in defining prebend.
|
DirectUnfoldBuilder.BodyList
The name list of bodies in current part.
|
DirectUnfoldBuilder.MatType
The material database defined in PDW.
|
DirectUnfoldBuilder.Types
Specifies the option of direct unfold type
|
DirectUnfoldCollection
Creates a
DirectUnfoldBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
DrawingSheetNameBuilder
Represents a
DrawingSheetNameBuilder To create a new instance of this class, use ToolingDrawingCollection.createDrawingSheetNameBuilder() Created in NX8.5.0 |
EdgePatchBuilder
Represents a builder to be used to create edge patch surfaces.
|
EdgePatchBuilder.BodyColorData
This class holds the data returned from
EdgePatchBuilder.getBodyColor() |
EdgePatchBuilder.PatchStatus
Settings of the patch status types.
|
EdgePatchBuilder.SelectTypes
Settings of the selection types.
|
EdgePatchCollection
Represents a collection of EdgePatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
EjectorPostProcessingBuilder
Represents a builder to be used to create Mold Wizard ejector post processing.
|
EjectorPostProcessingBuilder.TrimMethod
The processing type: Trim, Adjust length and Untrim.
|
EjectorPostProcessingBuilder.TrimPartName
The trim part where to find a trim surface as tool to trim ejector pins.
|
EjectorPostProcessingBuilder.TrimSufaceName
The trim surface types.
|
EjectorPostProcessingCollection
Creates a EjectorPostProcessingCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ElectrodeBlankBuilder
Design electrode blank builder to create an electrode blank for the selected body.
|
ElectrodeBlankBuilder.BlankMaterial
Represents the blank material option.
|
ElectrodeBlankBuilder.BlankShape
Represents the electrode blank shape option.
|
ElectrodeBlankBuilder.JointObject
Represents the transition type between head bodies and the blank.
|
ElectrodeCheckingBuilder
Electrode Checking builder to check the touch status of all electrode.
|
ElectrodeComponentBuilder
Electrode component builder to install holder and pallet.
|
ElectrodeComponentBuilder.Chuck
Represents the electrode chuck type.
|
ElectrodeCopyBuilder
The ElectrodeCopy builder
To create a new instance of this class, use ElectrodeCopyCollection.createElectrodeCopyBuilder() Default values. |
ElectrodeCopyBuilder.Copy
Represents an index to copy type
|
ElectrodeCopyCollection
Represents a collection of ElectrodeCopy builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ElectrodeDeleteBuilder
Electrode delete component builder to remove blank, pallet and holder from assembly.
|
ElectrodeDeleteBuilder.Types
delete sparking solid from blank or delete blank, pallet or holder directly.
|
ElectrodeDesignCollection
Represents a collection of Electrode Design.
|
ElectrodeInitializationBuilder
Electrode initialize project builder to creates an electrode design assembly.
|
EnlargeSurfaceBuilder
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges,
curves, datum planes or faces.
|
EnlargeSurfaceBuilder.ColorValueData
This class holds the data returned from
EnlargeSurfaceBuilder.getColorValue() |
EnlargeSurfaceBuilder.KeepDiscardOption
represents the keep discard options for selected region.
|
EnlargeSurfaceCollection
Represents a collection of Enlarge Surface
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EWDraftingBuilder
Represents the drafting builder which is used to create electrode drafting.
|
EWDraftingBuilder.CNCTemplateOption
the template option of cnc sheet type
|
EWDraftingBuilder.DrawingOption
the drawing type
|
EWDraftingBuilder.EDMTemplateOption
the template option of edm sheet type
|
EWDraftingBuilder.ModeOption
the drafting mode option
|
EWDraftingBuilder.NameOption
the drawing sheet name option
|
EWMultiPositionBuilder
Represents the multiple position builder which is used to get transformed electrode heads together.
|
EWMultiPositionCollection
Creates EWMultiPosition builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
FaceAttributeBuilder
Represents a builder to be used to create face attribute.
|
FaceColorManagementBuilder
Tooling builder to assign and edit color of objects
To create a new instance of this class, use FaceColorManagementCollection.createFaceColorManagementBuilder() Default values. |
FaceColorManagementBuilder.HoleTypeEnumValue
the hole type enumeration
|
FaceColorManagementCollection
Creates a
FaceColorManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
FaceSplitBuilder
Represents a face split operation
To create a new instance of this class, use FaceSplitCollection.createFaceSplitBuilder() Default values. |
FaceSplitBuilder.FaceSplitType
the type for Split Face
|
FaceSplitCollection
Creates Face Split collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FamilyMoldBuilder
Creates a Mold Wizard Family Mold builder
To create a new instance of this class, use FamilyMoldCollection.createFamilyMoldBuilder() Created in NX6.0.0 |
FamilyMoldCollection
Creates a
FamilyMoldCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
FastenerAssemConfigBuilder
Represents a Fastener Assem Config Collection.
|
FastenerAssemConfigCollection
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssy
Represents a
FastenerAssy
To create a new instance of this class, use FastenerAssyCollection.createBuilder() Created in NX5.0.0 |
FastenerAssy.HoleOperation
Represents the action on the hole menu of the fastener assembly.
|
FastenerAssy.ModeMethod
Represents adding and editing modes for the fastener assembly
|
FastenerAssy.SelectionObjectMethod
Represents selection object type
|
FastenerAssy.SelectionTypeMethod
Represents selection type for position and hole
|
FastenerAssy.StackTypeMethod
Represents screw_array type
|
FastenerAssyCollection
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssyCustomizationBuilder
Fastener assembly customization builder.
|
FastenerAssyCustomizationCollection
Represents a collection of FastenerAssyCustomizationBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FlowAnalysisBuilder
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder.AnalysisResults
The option of analysis results.
|
ForceCalculationBuilder
Represents a
ForceCalculationBuilder
Force Calculation Design is to calculate force of process
To create a new instance of this class, use ForceCalculationCollection.createForceCalculationBuilder() Default values. |
ForceCalculationBuilder.CalculationTypes
The calculation type.
|
ForceCalculationBuilder.ProcessTypes
The process type.
|
ForceCalculationCollection
Creates a
ForceCalculationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FormingInsertBuilder
Progressive Die Wizard builder to design forming punch and die insert
To create a new instance of this class, use FormingInsertCollection.createFormingInsertBuilder() Default values. |
FormingInsertBuilder.BlankPositions
Specifies the blank position.
|
FormingInsertBuilder.BlankTypes
Specifies the blank type.
|
FormingInsertBuilder.DesignOptions
Specifies the design type.
|
FormingInsertBuilder.ParentTypes
Specifies the parent part type.
|
FormingInsertCollection
Creates a
FormingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
GeneralInsertBuilder
General Insert Design Builder of PDW and EDW.
|
GeneralInsertBuilder.GenerateMethod
Specify the creation method of insert.
|
GeneralInsertBuilder.ParentOption
Specify the part parent of insert part.
|
GeneralInsertBuilder.Types
Specify the insert operation type.
|
GuidedExtensionBuilder
Builder for creating Guided Extension surface in NX
To create a new instance of this class, use GuidedExtensionManager.createBuilder() Default values. |
GuidedExtensionBuilder.SegmentType
Segment type for segments
|
GuidedExtensionManager
Represents the manager of the GuidedExtension builder
To obtain an instance of this class, refer to ToolingManager |
HemFixerBuilder
Hem Fixer Builder of PDW and EDW.
|
HoleManufacturingNoteBuilder
Tooling builder for HoleManufacturingNote
To create a new instance of this class, use HoleManufacturingNoteCollection.createHoleManufacturingNoteBuilder() Default values. |
HoleManufacturingNoteBuilder.DefineByViewOrHoles
the view selection or window selection type
|
HoleManufacturingNoteBuilder.HoleIndexType
the hole index type
|
HoleManufacturingNoteCollection
Creates a
HoleManufacturingNoteBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
InitProjBuilder
Represents a
InitProjBuilder
To create a new instance of this class, use InitProjCollection.createInitProjBuilder() Default values. |
InitProjBuilder.ProjTempOption
Represents the project template option of InitProj,
defines the pre-defined project template. this template will be used as the basic assembly structure for this new project
|
InitProjCollection
Represents a collection of InitProj
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjectBuilder
Mold Wizard initialize project builder
To create a new instance of this class, use InitProjectCollection.createBuilder() Default values. |
InitProjectBuilder.ConfigurationId
the configuration type includes default and orig
|
InitProjectBuilder.MaterialId
the material type includes None and Nylon
|
InitProjectBuilder.UnitId
the unit type includes metric and inch project type
|
InitProjectCollection
Represents a collection of InitProject builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertAuxiliaryBuilder
PDW insert auxiliary builder to design various auxiliaries of insert group
To create a new instance of this class, use InsertAuxiliaryCollection.createInsertAuxiliaryBuilder() Default values. |
InsertAuxiliaryBuilder.CircOperationTypes
Specifies the options of circular array.
|
InsertAuxiliaryBuilder.DesignToolOption
Specifies the design tool option.
|
InsertAuxiliaryBuilder.RectOperationOption
Specifies the rectangular array option.
|
InsertAuxiliaryBuilder.ShankShapeTypes
Specifies the shank shape.
|
InsertAuxiliaryBuilder.Types
Specifies the insert auxiliary type.
|
InsertAuxiliaryCollection
Creates a
InsertAuxiliaryBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
IntermediateStageBuilder
Represents a
IntermediateStageBuilder builder. |
IntermediateStageBuilder.DesignSequences
The types of design sequences
|
IntermediateStageBuilder.EditOptions
The types of changed intermediate stages
|
IntermediateStageBuilder.Orientations
The types of orientation of intermediate stages
|
IntermediateStageCollection
Creates a
IntermediateStageBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
LayoutBuilder
Represents a Tooling::LayoutBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutBuilder() Default values. |
LayoutBuilder.BalNumber
Represents the number of balance cavity.
|
LayoutBuilder.LayoutSubType
Represents the the sub type of layout.
|
LayoutBuilder.LayoutType
Represents the type of layout.
|
LayoutBuilder.XrefNum
Represents the type of x move refer.
|
LayoutBuilder.YrefNum
Represents the type of y move refer.
|
LayoutManagementBuilder
Layout Management Builder of Engineering Die Wizard
To create a new instance of this class, use LayoutManagementCollection.createLayoutManagementBuilder() Default values. |
LayoutManagementBuilder.StationItems
Specifies the station items
|
LayoutManagementCollection
Creates a
LayoutManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
LayoutRepositionBuilder
Represents a Tooling::LayoutRepositionBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutRepositionBuilder() Default values. |
LayoutRepositionBuilder.Method
Represents the type of layout transform.
|
LayoutRepositionBuilder.Type
Represents the method of layout transform.
|
LsdynaFormAnalysisResultDisplayBuilder
Represents a Ly-Dyna Formability Analysis - Result Display builder
To create a new instance of this class, use AutoDieCollection.createLsdynaFormAnalysisResultDisplayBuilder() Default values. |
LsdynaFormAnalysisResultDisplayBuilder.FormabilityStrainTypeName
Options to set strain type to display for formability analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StrainTypeName
Options to set strain type to display for strain analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName
Options to set stress type to display for stress analysis result.
|
LsdynaGeometryPreparationBuilder
Stamping Die LS-Dyna integration draw geometry preprare builder.
|
LsdynaGeometryPreparationBuilder.BlankOption
the enum of blank option.
|
LsdynaGeometryPreparationBuilder.BlankPosition
the enum of blank position.
|
LsdynaGeometryPreparationBuilder.ContactType
the enum of contact type.
|
LsdynaGeometryPreparationBuilder.DrawBeadType
the enum of draw bead type.
|
LsdynaGeometryPreparationBuilder.DrawType
the enum of draw type.
|
LsdynaGeometryPreparationBuilder.MaterialType
the enum of material type.
|
LsdynaGeometryPreparationBuilder.ProcessActionBinder
the enum of process action binder type.
|
LsdynaGeometryPreparationBuilder.ProcessActionDie
the enum of process action die type.
|
LsdynaGeometryPreparationBuilder.ProcessActionPunch
the enum of process action punch type.
|
LsdynaGeometryPreparationBuilder.ProcessType
the enum of process type.
|
LsdynaGeometryPreparationBuilder.TargetBinder
the enum of target binder type.
|
LsdynaGeometryPreparationBuilder.TargetDie
the enum of target die type.
|
LsdynaGeometryPreparationBuilder.TargetPunch
the enum of target punch type.
|
LsdynaKfileGeneratorBuilder
Represents LS-Dyna K file builder - K file generator builder
To create a new instance of this class, use AutoDieCollection.createLsdynaKfileGeneratorBuilder() Default values. |
LsdynaKfileGeneratorBuilder.MeshDataType
Types of data format.
|
LsdynaKfileGeneratorBuilder.MeshElementType
Types of mesh element type.
|
LsdynaKfileGeneratorBuilder.OperTypes
Types of operation.
|
ManufacturingGeometryBuilder
Represents a builder to be used to create manufacturing geometry.
|
ManufacturingGeometryCollection
Represents a collection of Manufacturing Geometry builder.
|
MoldCsysBuilder
Mold Wizard MoldCsys project builder
To create a new instance of this class, use MoldCsysCollection.createMoldCsysBuilder() Default values. |
MoldCsysBuilder.Wcsposition
Represents the method to computer the WCS positino
|
MoldCsysCollection
Creates a
MoldCsysCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldDesignCollection
Represents a collection of Mold Design.
|
MoldInsertBuilder
Mold Wizard mold insert management builder
To create a new instance of this class, use MoldInsertCollection.createMoldInsertBuilder() Default values. |
MoldInsertBuilder.BooleanType
design type: unite single workpieces, subtract overall workpieces
|
MoldInsertCollection
Creates a MoldInsertCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldProcessBuilder
Represents a Tooling::MoldProcessBuilder builder
To create a new instance of this class, use MoldProcessCollection.createMoldProcessBuilder() Default values. |
MoldProcessCollection
Represents a collection of Mold Process
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldwizardManager
Provides create builder methods for Moldwizard.
|
MotionSimulationBuilder
Represents a
MotionSimulationBuilder to support dynamic interference check. |
MotionSimulationBuilder.CamDefinitionType
Specifies the way to define cam, automatically or manually.
|
MotionSimulationBuilder.EjectorMoveOptions
Specifies the ejector move type, after or while
|
MotionSimulationBuilder.MoldbaseStyleType
Specifies the style type of moldbase, two-plate style or three-plate style
|
MotionSimulationBuilder.Types
Specifies the operation options of motion simulation.
|
MotionSimulationCollection
Represents a collection of MotionSimulation.
|
MWCopySheetsBuilder
Builder for copying sheets in the Mold Wizard application
To create a new instance of this class, use MWCopySheetsCollection.createBuilder() Default values. |
MWCopySheetsBuilder.Types
This enum represents the type of sheets to be copied
|
MWCopySheetsCollection
Represents a collection of MWCopySheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDefineRegionsBuilder
The MWDefineRegions builder
To create a new instance of this class, use MWDefineRegionsCollection.createBuilder() Default values. |
MWDefineRegionsBuilder.OrCreateEmptyRegionData
This class holds the data returned from
MWDefineRegionsBuilder.getOrCreateEmptyRegion() |
MWDefineRegionsBuilder.TranslucencyOptionType
This enum represents the translucency is to be performed on the selected or non-selected region faces
|
MWDefineRegionsCollection
Represents a collection of MWDefineRegions builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDefineSheetsBuilder
Builder for defining sheets in Mold Wizard
To create a new instance of this class, use MWDefineSheetsCollection.createBuilder() Default values. |
MWDefineSheetsCollection
Represents a collection of MWDefineSheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDesignGuideLinesBuilder
The builder for designing guide lines in Mold Wizard.
|
MWDesignGuideLinesBuilder.CreateGuideLineData
This class holds the data returned from
MWDesignGuideLinesBuilder.createGuideLine(nxopen.Curve, nxopen.Point3d, double) |
MWDesignGuideLinesBuilder.DirectionType
The type of direction for the guide line to be created.
|
MWDesignGuideLinesCollection
Represents a collection of MWDesignGuideLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDesignPartingSurfaceBuilder
The builder for designing parting surface in Mold Wizard.
|
MWDesignPartingSurfaceBuilder.ObjectType
The type of parting objects to be edited or placed.
|
MWDesignPartingSurfaceBuilder.PartingSurfaceType
The type of parting surface to be created.
|
MWDesignPartingSurfaceBuilder.TransitionSurfaceType
The type of transition surface to be created.
|
MWDesignPartingSurfaceBuilder.TrimAndExtendFromRegionType
The region type from which to trim and extend when creating parting surface.
|
MWDesignPartingSurfaceCollection
Represents a collection of MWDesignPartingSurface builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWLayoutCollection
Creates Mold Wizard layout collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWMoldedPartValidationBuilder
Represents a builder to be used to perform Molded Part Validation analysis.
|
MWMoldedPartValidationBuilder.AssignToRegion
Options for assigning faces to the Cavity or Core region
|
MWMoldedPartValidationBuilder.CalculateOption
Calculation options
|
MWMoldedPartValidationBuilder.CheckScope
Check scope for information
|
MWMoldedPartValidationBuilder.RangeType
Range type for displaying small corner radius faces
|
MWMoldedPartValidationManager
Represents a manager of the MWMoldedPartValidation builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
MWPartingManagerBuilder
Builder for the Parting Manager in the Mold Wizard application
To create a new instance of this class, use MWPartingManagerCollection.createBuilder() Created in NX7.5.0 |
MWPartingManagerBuilder.DataStatus
The status of the parting manager data.
|
MWPartingManagerBuilder.RegisterType
The type of registering UNDO identifier.
|
MWPartingManagerCollection
Represents a collection of MWPartingManager builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWSearchRegionBuilder
The Search Region builder is for defining a region by searching the region faces given a set of seed faces and boundary edges.
|
MWSearchRegionCollection
Represents a collection of MWSearchRegion builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWTraversePartingLinesBuilder
Builder for creating parting lines by traversing in the Mold Wizard application
To create a new instance of this class, use MWTraversePartingLinesCollection.createBuilder() Created in NX7.5.0 |
MWTraversePartingLinesCollection
Represents a collection of the MWTraversePartingLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ObjectAttributeManagementBuilder
Tooling builder to assign and edit attributes of objects
To create a new instance of this class, use ObjectAttributeManagementCollection.createObjectAttributeManagementBuilder() Default values. |
ObjectAttributeManagementBuilder.FilterAccordingToAttributeType
the selection filter type according to attribute
|
ObjectAttributeManagementBuilder.FilterType
the selection filter type
|
ObjectAttributeManagementBuilder.ShowComponentsType
the show type according to attribute
|
ObjectAttributeManagementBuilder.ShowType
show attributes of selected objects or show objects according to attribute
|
ObjectAttributeManagementCollection
Creates a
ObjectAttributeManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
OffsetCurve3DBuilder
Deprecated.
Deprecated in NX10.0.0. Please use
Offset3DCurveBuilder instead
|
PiercingInsertBuilder
Represents piercing insert builder.
|
PiercingInsertBuilder.AssociationToolType
Specifies the association tool operation option.
|
PiercingInsertBuilder.DieInsertTypeItems
Specifies the type of insert.
|
PiercingInsertBuilder.InsertPosition
Specifies the position of piercing inserts, for EDW only
|
PiercingInsertBuilder.NormalBbpslugType
Specifies the type of bottom plate slug.
|
PiercingInsertBuilder.NormalCavityType
Specifies the type of cavity.
|
PiercingInsertBuilder.NormalClearanceOptionType
Specifies the design option of piercing insert.
|
PiercingInsertBuilder.NormalDsslugType
Specifies the type of die shoe slug.
|
PiercingInsertBuilder.NormalOffsetSideType
Specifies the offset side of normal pierce insert design.
|
PiercingInsertBuilder.NormalUdpparentPartType
Specifies the parent part of user defined punch.
|
PiercingInsertBuilder.PunchPocketTypeItemsBP
Specifies the punch pocket type in backing plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsPP
Specifies the punch pocket type in punch plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsSP
Specifies the punch pocket type in stripper plate.
|
PiercingInsertBuilder.Types
Specifies the option of piercing insert type.
|
PiercingInsertCollection
Creates a
PiercingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PocketBuilder
Mold Wizard pocket management builder
To create a new instance of this class, use PocketCollection.createPocketBuilder() Created in NX6.0.0 |
PocketBuilder.ModeType
Represents the pocket operation method
|
PocketBuilder.RsetType
Represents the pocket refset types
|
PocketBuilder.ToolType
Represents the select type of tool
|
PocketCollection
Creates a
PocketBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PrebendBuilder.NumberBendsOption
The option of bend number to divide into
|
ProfileSplitBuilder
The ProfileSplit builder
To create a new instance of this class, use ProfileSplitCollection.createProfileSplitBuilder() Created in NX6.0.0 |
ProfileSplitCollection
Represents a collection of ProfileSplit builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ProgressiveDieManager
Provides create builder methods for Progressive Die.
|
QuickQuotationBuilder
Progressive Die Wizard builder to create quick quotation.
|
QuickQuotationBuilder.DesignTypes
Specify the design type.
|
QuickQuotationBuilder.InsertGroupMaterials
Specify the insert group material.
|
QuickQuotationBuilder.ManageTemporaryObjectsTypes
Specify the management type for the temporary objects.
|
QuickQuotationBuilder.ObjectTypes
Specify the concept sheet body type.
|
QuickQuotationBuilder.Types
Specify the operation type.
|
QuickQuotationCollection
Creates a
QuickQuotationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReferenceBlendBuilder
The ReferenceBlend builder
To create a new instance of this class, use ReferenceBlendCollection.createReferenceBlendBuilder() Created in NX7.0.0 |
ReferenceBlendCollection
Creates reference blend collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ReliefDesignBuilder
Represents a
ReliefDesignBuilder
Relief Design is to cut relief pocket for forming region . |
ReliefDesignBuilder.Method
The relief design creation method.
|
ReliefDesignBuilder.MethodOfDelete
The relief design delete method.
|
ReliefDesignBuilder.Types
The relief design type.
|
ReliefDesignCollection
Creates a
ReliefDesignBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
RemoveHolesBuilder
Remove Hole is used to patch holes for a solid body.
|
RemoveHolesBuilder.SelectionTypes
select object types, body or face
|
ReplaceSolidBuilder
Represents a replace solid operation.
|
ReplaceSolidCollection
Creates ReplaceSolidBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObject
Represents a
ReusableObject
To create a new instance of this class, use ToolingManager.createReusableObject() Created in NX7.5.2 |
ReusableObjectManager
Represents a collection of ReusableObject
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObjectPasteBuilder
Represents a
ReusableObjectPasteBuilder Use the ReusableObjectManager class to create a ReusableObjectPasteBuilder. |
ReusableObjectPasteBuilder.PasteMethods
Specifies the design option
|
ReusablePocketBuilder
Reusable pocket builder.
|
ReusablePocketBuilder.Hole
Represents hole types.
|
ReusablePocketCollection
Represents a collection of ReusablePocketBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunnerBuilder
Mold Wizard runner management builder, select curves as runner guide, choose section type and edit
section parameters, optional choose boolean type to create runner channel.
|
RunnerBuilder.GuideEndType
Represents the runner guide end type.
|
RunnerBuilder.SectionType
Represents the section type of runner channel.
|
RunnerCollection
Represents a collection of Runner
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunSimulationBuilder
Represents a
RunSimulationBuilder to animate the model,
analyze the collision and reference. null is returned To create a new instance of this class, use ProgressiveDieManager.createRunSimulationBuilder() Default values. |
ScrapDesignBuilder
Represents a scrap design builder
To create a new instance of this class, use ScrapDesignCollection.createScrapDesignBuilder() Default values. |
ScrapDesignBuilder.AddonType
Specifies the add-on type
|
ScrapDesignBuilder.Body
Specifies the operation type of scraps
|
ScrapDesignBuilder.DefScrapType
Specifies the definition type of scraps
|
ScrapDesignBuilder.EditScrapType
Specifies the edit type of scraps
|
ScrapDesignBuilder.OvercutType
Specifies the over cut type, different type has different parameters
|
ScrapDesignBuilder.RemoveType
Specifies the removing type as filter
|
ScrapDesignBuilder.ScrapDefPosition
Specifies the position method of scraps, projecting method is normally used
|
ScrapDesignBuilder.ScrapDefType
Specifies the creation type of scraps
|
ScrapDesignBuilder.TrimNumType
Specifies the step of trimming process, the maximum is five
|
ScrapDesignCollection
Represents a collection of ScrapDesign
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SectionLineCreationBuilder
Represents a
SectionLineCreationBuilder which is
used to create or edit the section line creation. |
SelectReuseLibraryItemBuilder
Select a part from the reuse library .
|
SelectReuseLibraryListItemBuilder
Select reuse library list item .
|
SelectReuseLibraryListItemBuilderList
Represents a list of objects.
|
ShimBuilder
Shim Builder of PDW and EDW.
|
ShimBuilder.ParentOption
Specify the parent node.
|
ShimBuilder.Types
Specify the shim operation type.
|
ShimInnerProfileSetBuilder
This is a seed block of set list.
|
ShimInnerProfileSetBuilderList
Represents a list of objects.
|
SIZERCollection
Represents a collection of SIZER
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
SlugRetentionBuilder
Represents a
SlugRetentionBuilder which is used to create the Slug Retention. |
SolidPatchBuilder
Represents a builder to be used to create a solid patch.
|
SolidPatchBuilder.SolidPatchType
Settings of the solid patch creation types.
|
SolidPatchCollection
Represents a collection of SolidPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SpecifyBaffleBuilder
Represents a builder to be used to create specify baffle.
|
SpecifyBaffleBuilder.AttributeTypes
Types to specify how to assign attributes to the selected body.
|
SpecifyBaffleBuilder.ChannelColorData
This class holds the data returned from
SpecifyBaffleBuilder.getChannelColor() |
SpecifyBaffleCollection
Represents a collection of Specify Baffle builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpecifyCircuitBuilder
Represents a builder to be used to create specify circuit.
|
SpecifyCircuitCollection
Represents a collection of Specify Circuit builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SplitSolidBuilder
Represents a builder to be used to split a solid with geometry tools.
|
SplitSolidBuilder.OperationType
the split operation type: split, trim.
|
SplitSolidBuilder.ToolObjectOption
the split tool selection type: Existing Object, New Plane.
|
SplitSolidCollection
Creates SplitSolid builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
SpreadsheetData
Represents the spreadsheet.
|
SpreadsheetData.DefinedAttributesExpressionsData
This class holds the data returned from
SpreadsheetData.getDefinedAttributesExpressions(nxopen.tooling.SpreadsheetData.KeywordType) |
SpreadsheetData.KeywordType
Represents the different attribute or expression section in spreadsheet
|
SpreadsheetData.ParameterStatus
Represents the different spreadsheet parameter status
|
SpreadsheetDataParameter
Represents parameter in the spreadsheet.
|
SpreadsheetDataParameter.Status
Represents the different spreadsheet parameter status
|
StandardPartBuilder
Represents a builder to be used to create Mold Wizard Standard Part.
|
StandardPartBuilder.EditType
Represents the type to edit a standard part.
|
StandardPartBuilder.RefsetName
Represents the reference set of the standard part when it is added to the assembly.
|
StandardPartCollection
Creates a StandardPartCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
StandardPartPositionBuilder
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position.
|
StandardPartPositionCollection
Creates a StandardPartPositionCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
StockSizeCollection
Represents a collection of StockSize
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
StripLayoutBuilder
Represents a
StripLayoutBuilder
This class is for Strip Layout Design UI
To create a new instance of this class, use StripLayoutCollection.createStripLayoutBuilder() Created in NX6.0.0 |
StripLayoutBuilder.FromStationType
Specifies the option of From Station for layout
|
StripLayoutBuilder.ToStationType
Specifies the option of To Station for layout
|
StripLayoutCollection
Contains the create functions for builders.
|
StripLayoutStationInformationBuilder
Strip Layout Process Description Builder of Tooling.
|
StripperVentingBuilder
Stripper Venting Builder of PDW and EDW.
|
SubInsertBuilder
The SubInsert builder
To create a new instance of this class, use SubInsertCollection.createSubInsertBuilder() Default values. |
SubInsertBuilder.Shape
Represents the foot shape
|
SubInsertBuilder.Types
Represents the type of parent part
|
SubInsertCollection
Creates SubInsert builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ToolingApplication
Wizard type, some of them should be same as in mpdwshare_uf_mold.h
|
ToolingCloneaction
Clone action type
|
ToolingClonemethod
Clone method
|
ToolingCloneparttype
Part file type, .sim, .fem etc.
|
ToolingDrawingCollection
Creates a
CompDrawingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
TraverseLoopBuilder
The builder class for Traverse Loop component which assists you
to select or traverse a string of adjacent curves or edges.
|
TraverseLoopBuilder.CheckGapData
This class holds the data returned from
TraverseLoopBuilder.checkGap(nxopen.NXObject[]) |
TraverseLoopCollection
Represents a collection of TraverseLoopbuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimMoldComponentsBuilder
Represents a builder to be used to create Mold Wizard trim mold components.
|
TrimMoldComponentsBuilder.TargetScope
the target bodies selection scope
|
TrimMoldComponentsBuilder.TrimMethod
the processing type of Trim Mold Components.
|
TrimMoldComponentsBuilder.TrimPartName
the trim part options where a part chosen to work around
|
TrimMoldComponentsBuilder.TrimSurfaceName
trim surface types
|
TrimMoldComponentsCollection
Creates a TrimMoldComponentsCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimRegionBuilder
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies.
|
TrimRegionBuilder.BoundaryOption
represents the boundary type option, body/curve type or traverse type.
|
TrimRegionBuilder.ColorValueData
This class holds the data returned from
TrimRegionBuilder.getColorValue() |
TrimRegionBuilder.RegionOption
represents the option to keep or discard the selected region.
|
TrimRegionCollection
Represents a collection of Trim Region
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimSolidBuilder
Mold Wizard trim solid management builder, trims bounding box body with region, subtract
bounding box with workpiece or keep region and box.
|
TrimSolidBuilder.TrimSolidAction
represents the action to create trim solid.
|
TrimSolidBuilder.Types
represents the option to select face or sheet body or manufacturing faces to trim the bounding box.
|
TrimSolidCollection
Represents a collection of Trim Solid
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
UndersizeCollection
Creates a undersize builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
UnfoldingSimulationBuilder
Unfolding Simulation Builder of PDW and EDW.
|
UniversalUnformBuilder.BendTypes
The types of bend
|
UnusedFileManagementBuilder
Represents a
UnusedFileManagementBuilder
Unused File Management is to manage the unused files of the project. |
UnusedFileManagementBuilder.FileDirectory
the unused file location.
|
UnusedFileManagementCollection
Creates a
UnusedFileManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
ValidCheckBuilder
This is the JA builder for static interference check
To create a new instance of this class, use ValidCheckCollection.createValidCheckBuilder() Default values. |
ValidCheckBuilder.AnalysisMode
the analysis mode, including solid-based mode and facet-based mode
|
ValidCheckBuilder.CheckingType
the checking type, including true body, false body or both
|
ValidCheckBuilder.SelMode
the selection type, including component and solid body
|
ValidCheckCollection
Represents a collection of ValidCheck
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WallThicknessCheckerBuilder
Represents a builder to be used to perform wall thickness analysis.
|
WallThicknessCheckerBuilder.CalculateMethod
The calculation method used for the wall thickness analysis.
|
WallThicknessCheckerBuilder.LegendControl
The legend control used in displaying the thickness results.
|
WallThicknessCheckerBuilder.RangeType
The range type for defining the ranges used in displaying the thickness results.
|
WallThicknessCheckerManager
Represents the manager of the WallThicknessChecker builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WireHoleBuilder
Represents a
WireHoleBuilder
This class is for Wire Hole Design UI
To create a new instance of this class, use WireHoleCollection.createWireHoleBuilder() Default values. |
WireHoleCollection
Creates a
WireHoleBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WorkflowManagementCollection
Creates a Workflow Management Collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WorkpieceBuilder
Mold Wizard work piece builder
To create a new instance of this class, use WorkpieceCollection.createWorkpieceBuilder() Default values. |
WorkpieceBuilder.MethodType
the unit type includes the work piece define method
|
WorkpieceBuilder.Types
the unit type includes product and combined work piece type
|
WorkpieceBuilder.WorkPieceType
the unit type includes the work piece create method
|
WorkpieceCollection
Creates a Workpiece Collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.