Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.FIFTH
the snap size is 0.2
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.FIVE
the snap size is 5
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.HALF
the snap size is 1/2
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.ONE
the snap size is 1
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.TEN
the snap size is 10
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.TENTH
the snap size is 0.1
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.TWO
the snap size is 2
|
Modifier and Type | Method and Description |
---|---|
BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.snapSize()
Returns the option to set the increment of the scale bar.
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlankLayoutBuilder.SnapSizeOption |
BlankLayoutBuilder.SnapSizeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlankLayoutBuilder.SnapSizeOption[] |
BlankLayoutBuilder.SnapSizeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BlankLayoutBuilder.setSnapSize(BlankLayoutBuilder.SnapSizeOption snapSize)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.