Interface | Description |
---|---|
AddReusableFeatureCollection |
Represents a collection of AddReusableFeature
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
AddReusablePart |
Represents a
AddReusablePart
To create a new instance of this class, use AddReusablePartCollection.createBuilder() Created in NX5.0.0 |
AddReusablePartCollection |
Represents a collection of AddReusablePart
To obtain an instance of this class, refer to Part Created in NX5.0.0 |
AssemblyDrawingBuilder |
Represents a
AssemblyDrawingBuilder which is
used to create or edit the Assembly Drawing. |
AssignPatchBuilder |
Represents a builder to be used to add sheet bodies as patch surfaces or delete patch surfaces.
|
AssignPatchCollection |
Represents a collection of AssignPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
AutoDieCollection |
Represents a collection of Die Design Draw Punch
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
AutoDimensionBuilder |
Represents a
AutoDimensionBuilder which is
used to create or edit the Auto Dimension. |
BackingPadBuilder |
Represents a
BackingPadBuilder which is used to create or delete the Backing Pad. |
BendInsertDesignBuilder |
Represents a
BendInsertDesignBuilder
Bend Insert Design is to create inset puch or die for bend . |
BendInsertDesignCollection |
Creates a
BendInsertDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BendOperationBuilder |
Represents a
BendOperationBuilder builder. |
BendOperationCollection |
Creates a
BendOperationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlankGeneratorBuilder |
Represents a
BlankGeneratorBuilder
This class is for Blank Generator Design UI
To create a new instance of this class, use BlankGeneratorCollection.createBlankGeneratorBuilder() Created in NX7.5.0 |
BlankGeneratorCollection |
Creates a
BlankGeneratorBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
BlankLayoutBuilder |
Progressive Die Wizard blank layout builder
To create a new instance of this class, use BlankLayoutCollection.createBlankLayoutBuilder() Default values. |
BlankLayoutCollection |
Creates a
BlankLayoutBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
BlankNestingBuilder |
Blank Nesting Builder of PDW, EDW and Die Engineering.
|
BlankNestingCollection |
Creates a
BlankNestingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
BlendCurve3DBuilder |
Represents a
BlendCurve3DBuilder builder which implements
blend curves in one side where the corner radius is too small. |
BomBuilder |
Represents a Tooling::BomBuilder builder
To create a new instance of this class, use BomCollection.createBomBuilder() Default values. |
BomCollection |
Represents a collection of Bom
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
BomListBuilder |
Represents a
BomListBuilder builder. |
BurringInsertBuilder |
Progressive Die Wizard builder to design burring punch and die insert
To create a new instance of this class, use BurringInsertCollection.createBurringInsertBuilder() Default values. |
BurringInsertCollection |
Creates a
BurringInsertCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CaeReuseLibrary |
Represents a
CaeReuseLibrary
To obtain an instance of this class, refer to BaseFEModel Created in NX7.5.2 |
CalculateAreaBuilder |
The CalculateArea builder
To create a new instance of this class, use CalculateAreaCollection.createBuilder() Default values. |
CalculateAreaCollection |
Represents a collection of CalculateArea builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
CAMDataManager |
Represents an object that manages cam data objects.
|
ChangeoverManagementBuilder |
Represents a
ChangeoverManagementBuilder to support changeover workflow management. |
ChannelAdjustBuilder |
The builder class for Channel Adjust which assists you
to adjust the postion and the length of the channel.
|
ChannelAdjustCollection |
Creates a ChannelAdjust Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ChannelFittingBuilder |
The builder class for Channel Fitting which assists you
to add cooling fitting.
|
ChannelFittingCollection |
Creates a ChannelFitting Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ClearanceManagementBuilder |
Progressive Die Wizard builder to management clearances.
|
ClearanceManagementCollection |
Creates a
ClearanceManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
CloneObject |
Represents the clone operation in Add Reusable Component Builder.
|
ClonePart |
Represents the part inforamtion to be cloned in Add Reusable Component Builder.
|
CompDrawingBuilder |
Represents a
CompDrawingBuilder which is
used to create or edit the Component Drawing. |
ConceptPositionBuilder |
concept position builder for standard part design
To create a new instance of this class, use ConceptPositionCollection.createConceptPositionBuilder() Created in NX6.0.0 |
ConceptPositionCollection |
Represents a collection of ConceptPosition
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ConcurrentDesignManagementBuilder |
Represents a
ConcurrentDesignManagementBuilder to support concurrent design workflow management. |
CoolingConnectBuilder |
The builder class for Cooling connection which assists you
to create channel and connect it to other channels.
|
CoolingConnectCollection |
Creates a CoolingConnect Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingDefineChannelBuilder |
The builder class for Cooling Define Channel which assists you
to create channels directly.
|
CoolingDefineChannelCollection |
Creates a CoolingDefineChannel Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
CoolingExtendBuilder |
The builder class for Channel Extend which assists you
to extend the channel.
|
CoolingExtendCollection |
Creates a CoolingExtend Collection.
|
CoolingFittingData |
Represents the cooling fitting data in Add Channel Fitting Builder.
|
CoolingPatternBuilder |
The builder class for Cooling pattern which assists you
to create channels with selected curves.
|
CoolingPatternCollection |
Creates a CoolingPattern Collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CornerDesignBuilder |
Represents a
CornerDesignBuilder ,
Corner Design is to provide tools to make corner. |
CornerDesignCollection |
Creates a
CornerDesignCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
CreateBoxBuilder |
Represents a box creation operation
To create a new instance of this class, use CreateBoxCollection.createBoxBuilder(nxopen.NXObject) Default values. |
CreateBoxCollection |
Creates CreateBoxBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DefineCamBuilder |
Represents a
DefineCamBuilder to create different types of cam objects, which
are used for kinematic motion To create a new instance of this class, use ProgressiveDieManager.createDefineCamBuilder() Default values. |
DefineLifterBuilder |
Represents a
DefineLifterBuilder to create different types of lifter objects, which
are used for kinematic motion. |
DefineNeutralFactorBuilder |
Represeents a
DefineNeutralFactorBuilder to define
neutral factor according to material and formula in the spreadsheet table. |
DesignTrimToolBuilder |
Represents a builder to be used to create Mold Wizard design trim tool.
|
DesignTrimToolCollection |
Creates a DesignTrimToolCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
DieBaseBuilder |
Represents Progressive Die Wizard and Engineering Die Wizard builder to manage die base.
|
DieBaseCollection |
Creates a
DieBaseCollection To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
DieDesDrawDieBuilder |
Represents the Die Design draw die management builder, which is to create a draw die by selected
sheet body, curve and base plane.
|
DieDesDrawPunchBuilder |
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve
and base plane.
|
DieDesignLowerBinderBuilder |
Represents a Lower Binder builder
To create a new instance of this class, use AutoDieCollection.createDieDesignLowerBinderBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesignSettingBuilder |
Represents a
DieDesignSettingBuilder
This class is for Die Design Setting UI
To create a new instance of this class, use DieDesignSettingCollection.createDieDesignSettingBuilder() Created in NX7.5.0 |
DieDesignSettingCollection |
Creates a
DieDesignSettingBuilder . |
DieDesignTrimPostBuilder |
Represents a Trim Post builder
To create a new instance of this class, use AutoDieCollection.createDieDesignTrimPostBuilder(nxopen.features.Feature) Created in NX9.0.0 |
DieDesPierceInsertBuilder |
Represents Die Design Pierce Insert builder.
|
DieEngFormTaskBuilder |
Represents a Form Task builder
To create a new instance of this class, use AutoDieCollection.createDieEngFormTaskBuilder(nxopen.features.Feature) Default values. |
DieEngProcessUpdateManagerBuilder |
Die Engineer process update manager management builder.
|
DieEngStampingCarryoverBuilder |
Represents a Stamping Carryover builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingCarryoverBuilder(nxopen.features.BodyFeature) Created in NX10.0.0 |
DieEngStampingOutputBuilder |
Represents a Stamping Output builder
To create a new instance of this class, use AutoDieCollection.createDieEngStampingOutputBuilder(nxopen.features.BodyFeature) Default values. |
DieEngTrimAngleCheck |
Represents a die engineering trim angle check analysis object
To create or edit an instance of this class, use DieEngTrimAngleCheckBuilder Created in NX8.5.0 |
DieEngTrimAngleCheckBuilder |
Represents a Trim Angle Check builder
To create a new instance of this class, use AutoDieCollection.createDieEngTrimAngleCheckBuilder(nxopen.geometricanalysis.AnalysisObject) Default values. |
DieEngTrimTaskBuilder |
Die Engineer trim task management builder, create a trim task by selected die tip, trim bounds,
start plane and end plane.
|
DirectUnbendBuilder |
The builder contains all inputs for direct unbend.
|
DirectUnfoldBuilder |
The builder contains all inputs for direct unfolding.
|
DirectUnfoldCollection |
Creates a
DirectUnfoldBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
DrawingSheetNameBuilder |
Represents a
DrawingSheetNameBuilder To create a new instance of this class, use ToolingDrawingCollection.createDrawingSheetNameBuilder() Created in NX8.5.0 |
EdgePatchBuilder |
Represents a builder to be used to create edge patch surfaces.
|
EdgePatchCollection |
Represents a collection of EdgePatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
EjectorPostProcessingBuilder |
Represents a builder to be used to create Mold Wizard ejector post processing.
|
EjectorPostProcessingCollection |
Creates a EjectorPostProcessingCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EjectorTableData |
Represents the ejector table data in Ejector Table Builder.
|
ElectrodeBlankBuilder |
Design electrode blank builder to create an electrode blank for the selected body.
|
ElectrodeCheckingBuilder |
Electrode Checking builder to check the touch status of all electrode.
|
ElectrodeComponentBuilder |
Electrode component builder to install holder and pallet.
|
ElectrodeCopyBuilder |
The ElectrodeCopy builder
To create a new instance of this class, use ElectrodeCopyCollection.createElectrodeCopyBuilder() Default values. |
ElectrodeCopyCollection |
Represents a collection of ElectrodeCopy builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ElectrodeDeleteBuilder |
Electrode delete component builder to remove blank, pallet and holder from assembly.
|
ElectrodeDesign |
Represents an Electrode Design.
|
ElectrodeDesignCollection |
Represents a collection of Electrode Design.
|
ElectrodeInitializationBuilder |
Electrode initialize project builder to creates an electrode design assembly.
|
EnlargeSurfaceBuilder |
Mold Wizard enlarge surface management builder, trims a enlarged surface to a boundary of edges,
curves, datum planes or faces.
|
EnlargeSurfaceCollection |
Represents a collection of Enlarge Surface
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
EWDraftingBuilder |
Represents the drafting builder which is used to create electrode drafting.
|
EWMultiPositionBuilder |
Represents the multiple position builder which is used to get transformed electrode heads together.
|
EWMultiPositionCollection |
Creates EWMultiPosition builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
FaceAttributeBuilder |
Represents a builder to be used to create face attribute.
|
FaceColorManagementBuilder |
Tooling builder to assign and edit color of objects
To create a new instance of this class, use FaceColorManagementCollection.createFaceColorManagementBuilder() Default values. |
FaceColorManagementCollection |
Creates a
FaceColorManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
FaceSplitBuilder |
Represents a face split operation
To create a new instance of this class, use FaceSplitCollection.createFaceSplitBuilder() Default values. |
FaceSplitCollection |
Creates Face Split collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FamilyMoldBuilder |
Creates a Mold Wizard Family Mold builder
To create a new instance of this class, use FamilyMoldCollection.createFamilyMoldBuilder() Created in NX6.0.0 |
FamilyMoldCollection |
Creates a
FamilyMoldCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
FastenerAssemConfigBuilder |
Represents a Fastener Assem Config Collection.
|
FastenerAssemConfigCollection |
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssy |
Represents a
FastenerAssy
To create a new instance of this class, use FastenerAssyCollection.createBuilder() Created in NX5.0.0 |
FastenerAssyCollection |
Represents a collection of FastenerAssy
To obtain an instance of this class, refer to ToolingManager Created in NX5.0.0 |
FastenerAssyCustomizationBuilder |
Fastener assembly customization builder.
|
FastenerAssyCustomizationCollection |
Represents a collection of FastenerAssyCustomizationBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
FlowAnalysisBuilder |
Represents the builder which is used to create flow analysis.
|
FlowDisplayBuilder |
Represents the builder which is used to create flow analysis.
|
ForceCalculationBuilder |
Represents a
ForceCalculationBuilder
Force Calculation Design is to calculate force of process
To create a new instance of this class, use ForceCalculationCollection.createForceCalculationBuilder() Default values. |
ForceCalculationCollection |
Creates a
ForceCalculationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
FormingInsertBuilder |
Progressive Die Wizard builder to design forming punch and die insert
To create a new instance of this class, use FormingInsertCollection.createFormingInsertBuilder() Default values. |
FormingInsertCollection |
Creates a
FormingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
GeneralInsertBuilder |
General Insert Design Builder of PDW and EDW.
|
GuidedExtensionBuilder |
Builder for creating Guided Extension surface in NX
To create a new instance of this class, use GuidedExtensionManager.createBuilder() Default values. |
GuidedExtensionManager |
Represents the manager of the GuidedExtension builder
To obtain an instance of this class, refer to ToolingManager |
HemFixerBuilder |
Hem Fixer Builder of PDW and EDW.
|
HoleManufacturingNoteBuilder |
Tooling builder for HoleManufacturingNote
To create a new instance of this class, use HoleManufacturingNoteCollection.createHoleManufacturingNoteBuilder() Default values. |
HoleManufacturingNoteCollection |
Creates a
HoleManufacturingNoteBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
InitProjBuilder |
Represents a
InitProjBuilder
To create a new instance of this class, use InitProjCollection.createInitProjBuilder() Default values. |
InitProjCollection |
Represents a collection of InitProj
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InitProjectBuilder |
Mold Wizard initialize project builder
To create a new instance of this class, use InitProjectCollection.createBuilder() Default values. |
InitProjectCollection |
Represents a collection of InitProject builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
InsertAuxiliaryBuilder |
PDW insert auxiliary builder to design various auxiliaries of insert group
To create a new instance of this class, use InsertAuxiliaryCollection.createInsertAuxiliaryBuilder() Default values. |
InsertAuxiliaryCollection |
Creates a
InsertAuxiliaryBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
IntermediateStageBuilder |
Represents a
IntermediateStageBuilder builder. |
IntermediateStageCollection |
Creates a
IntermediateStageBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
LayoutBuilder |
Represents a Tooling::LayoutBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutBuilder() Default values. |
LayoutManagementBuilder |
Layout Management Builder of Engineering Die Wizard
To create a new instance of this class, use LayoutManagementCollection.createLayoutManagementBuilder() Default values. |
LayoutManagementCollection |
Creates a
LayoutManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
LayoutRepositionBuilder |
Represents a Tooling::LayoutRepositionBuilder builder
To create a new instance of this class, use MWLayoutCollection.createLayoutRepositionBuilder() Default values. |
LsdynaFormAnalysisResultDisplayBuilder |
Represents a Ly-Dyna Formability Analysis - Result Display builder
To create a new instance of this class, use AutoDieCollection.createLsdynaFormAnalysisResultDisplayBuilder() Default values. |
LsdynaGeometryPreparationBuilder |
Stamping Die LS-Dyna integration draw geometry preprare builder.
|
LsdynaKfileGeneratorBuilder |
Represents LS-Dyna K file builder - K file generator builder
To create a new instance of this class, use AutoDieCollection.createLsdynaKfileGeneratorBuilder() Default values. |
ManufacturingGeometryBuilder |
Represents a builder to be used to create manufacturing geometry.
|
ManufacturingGeometryCollection |
Represents a collection of Manufacturing Geometry builder.
|
MoldCsysBuilder |
Mold Wizard MoldCsys project builder
To create a new instance of this class, use MoldCsysCollection.createMoldCsysBuilder() Default values. |
MoldCsysCollection |
Creates a
MoldCsysCollection To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldDesign |
Represents an Mold Design.
|
MoldDesignCollection |
Represents a collection of Mold Design.
|
MoldInsertBuilder |
Mold Wizard mold insert management builder
To create a new instance of this class, use MoldInsertCollection.createMoldInsertBuilder() Default values. |
MoldInsertCollection |
Creates a MoldInsertCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldProcessBuilder |
Represents a Tooling::MoldProcessBuilder builder
To create a new instance of this class, use MoldProcessCollection.createMoldProcessBuilder() Default values. |
MoldProcessCollection |
Represents a collection of Mold Process
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MoldwizardManager |
Provides create builder methods for Moldwizard.
|
MotionSimulationBuilder |
Represents a
MotionSimulationBuilder to support dynamic interference check. |
MotionSimulationCollection |
Represents a collection of MotionSimulation.
|
MWCopySheetsBuilder |
Builder for copying sheets in the Mold Wizard application
To create a new instance of this class, use MWCopySheetsCollection.createBuilder() Default values. |
MWCopySheetsCollection |
Represents a collection of MWCopySheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDefineRegionsBuilder |
The MWDefineRegions builder
To create a new instance of this class, use MWDefineRegionsCollection.createBuilder() Default values. |
MWDefineRegionsCollection |
Represents a collection of MWDefineRegions builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDefineSheetsBuilder |
Builder for defining sheets in Mold Wizard
To create a new instance of this class, use MWDefineSheetsCollection.createBuilder() Default values. |
MWDefineSheetsCollection |
Represents a collection of MWDefineSheets builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWDesignGuideLinesBuilder |
The builder for designing guide lines in Mold Wizard.
|
MWDesignGuideLinesCollection |
Represents a collection of MWDesignGuideLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWDesignPartingSurfaceBuilder |
The builder for designing parting surface in Mold Wizard.
|
MWDesignPartingSurfaceCollection |
Represents a collection of MWDesignPartingSurface builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWLayoutCollection |
Creates Mold Wizard layout collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWMoldedPartValidationBuilder |
Represents a builder to be used to perform Molded Part Validation analysis.
|
MWMoldedPartValidationManager |
Represents a manager of the MWMoldedPartValidation builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
MWPartingManagerBuilder |
Builder for the Parting Manager in the Mold Wizard application
To create a new instance of this class, use MWPartingManagerCollection.createBuilder() Created in NX7.5.0 |
MWPartingManagerCollection |
Represents a collection of MWPartingManager builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
MWSearchRegionBuilder |
The Search Region builder is for defining a region by searching the region faces given a set of seed faces and boundary edges.
|
MWSearchRegionCollection |
Represents a collection of MWSearchRegion builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
MWTraversePartingLinesBuilder |
Builder for creating parting lines by traversing in the Mold Wizard application
To create a new instance of this class, use MWTraversePartingLinesCollection.createBuilder() Created in NX7.5.0 |
MWTraversePartingLinesCollection |
Represents a collection of the MWTraversePartingLines builder
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ObjectAttributeManagementBuilder |
Tooling builder to assign and edit attributes of objects
To create a new instance of this class, use ObjectAttributeManagementCollection.createObjectAttributeManagementBuilder() Default values. |
ObjectAttributeManagementCollection |
Creates a
ObjectAttributeManagementBuilder To obtain an instance of this class, refer to ToolingManager Created in NX9.0.0 |
OffsetCurve3DBuilder | Deprecated
Deprecated in NX10.0.0.
|
PiercingInsertBuilder |
Represents piercing insert builder.
|
PiercingInsertCollection |
Creates a
PiercingInsertBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PocketBuilder |
Mold Wizard pocket management builder
To create a new instance of this class, use PocketCollection.createPocketBuilder() Created in NX6.0.0 |
PocketCollection |
Creates a
PocketBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
PrebendBuilder |
Represents a
PrebendBuilder builder to divide bend faces. |
ProfileSplitBuilder |
The ProfileSplit builder
To create a new instance of this class, use ProfileSplitCollection.createProfileSplitBuilder() Created in NX6.0.0 |
ProfileSplitCollection |
Represents a collection of ProfileSplit builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ProgressiveDieManager |
Provides create builder methods for Progressive Die.
|
QuickQuotationBuilder |
Progressive Die Wizard builder to create quick quotation.
|
QuickQuotationCollection |
Creates a
QuickQuotationBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReferenceBlendBuilder |
The ReferenceBlend builder
To create a new instance of this class, use ReferenceBlendCollection.createReferenceBlendBuilder() Created in NX7.0.0 |
ReferenceBlendCollection |
Creates reference blend collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
ReliefDesignBuilder |
Represents a
ReliefDesignBuilder
Relief Design is to cut relief pocket for forming region . |
ReliefDesignCollection |
Creates a
ReliefDesignBuilder To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
RemoveHolesBuilder |
Remove Hole is used to patch holes for a solid body.
|
ReplaceSolidBuilder |
Represents a replace solid operation.
|
ReplaceSolidCollection |
Creates ReplaceSolidBuilder collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObject |
Represents a
ReusableObject
To create a new instance of this class, use ToolingManager.createReusableObject() Created in NX7.5.2 |
ReusableObjectManager |
Represents a collection of ReusableObject
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ReusableObjectPasteBuilder |
Represents a
ReusableObjectPasteBuilder Use the ReusableObjectManager class to create a ReusableObjectPasteBuilder. |
ReusablePocketBuilder |
Reusable pocket builder.
|
ReusablePocketCollection |
Represents a collection of ReusablePocketBuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunnerBuilder |
Mold Wizard runner management builder, select curves as runner guide, choose section type and edit
section parameters, optional choose boolean type to create runner channel.
|
RunnerCollection |
Represents a collection of Runner
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
RunSimulationBuilder |
Represents a
RunSimulationBuilder to animate the model,
analyze the collision and reference. null is returned To create a new instance of this class, use ProgressiveDieManager.createRunSimulationBuilder() Default values. |
ScrapDesignBuilder |
Represents a scrap design builder
To create a new instance of this class, use ScrapDesignCollection.createScrapDesignBuilder() Default values. |
ScrapDesignCollection |
Represents a collection of ScrapDesign
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SectionLineCreationBuilder |
Represents a
SectionLineCreationBuilder which is
used to create or edit the section line creation. |
SelectReuseLibraryItemBuilder |
Select a part from the reuse library .
|
SelectReuseLibraryListBuilder |
Select a list of objects from the reuse library .
|
SelectReuseLibraryListItemBuilder |
Select reuse library list item .
|
SelectReuseLibraryListItemBuilderList |
Represents a list of objects.
|
ShimBuilder |
Shim Builder of PDW and EDW.
|
ShimInnerProfileSetBuilder |
This is a seed block of set list.
|
ShimInnerProfileSetBuilderList |
Represents a list of objects.
|
SIZERCollection |
Represents a collection of SIZER
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
SlugRetentionBuilder |
Represents a
SlugRetentionBuilder which is used to create the Slug Retention. |
SolidPatchBuilder |
Represents a builder to be used to create a solid patch.
|
SolidPatchCollection |
Represents a collection of SolidPatch builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
SpecifyBaffleBuilder |
Represents a builder to be used to create specify baffle.
|
SpecifyBaffleCollection |
Represents a collection of Specify Baffle builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SpecifyCircuitBuilder |
Represents a builder to be used to create specify circuit.
|
SpecifyCircuitCollection |
Represents a collection of Specify Circuit builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
SplitSolidBuilder |
Represents a builder to be used to split a solid with geometry tools.
|
SplitSolidCollection |
Creates SplitSolid builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX7.0.0 |
SpreadsheetData |
Represents the spreadsheet.
|
SpreadsheetDataParameter |
Represents parameter in the spreadsheet.
|
StandardPartBuilder |
Represents a builder to be used to create Mold Wizard Standard Part.
|
StandardPartCollection |
Creates a StandardPartCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
StandardPartPositionBuilder |
Represents a StandardPartPositionBuilder to add or edit a standard part in the selected plane with specified position.
|
StandardPartPositionCollection |
Creates a StandardPartPositionCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX8.5.0 |
StockSizeCollection |
Represents a collection of StockSize
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
StripLayoutBuilder |
Represents a
StripLayoutBuilder
This class is for Strip Layout Design UI
To create a new instance of this class, use StripLayoutCollection.createStripLayoutBuilder() Created in NX6.0.0 |
StripLayoutCollection |
Contains the create functions for builders.
|
StripLayoutStationInformationBuilder |
Strip Layout Process Description Builder of Tooling.
|
StripperVentingBuilder |
Stripper Venting Builder of PDW and EDW.
|
SubInsertBuilder |
The SubInsert builder
To create a new instance of this class, use SubInsertCollection.createSubInsertBuilder() Default values. |
SubInsertCollection |
Creates SubInsert builder collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
ToolingDrawingCollection |
Creates a
CompDrawingBuilder To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
ToolingManager |
Contains the collection objects for creating and iterating over Reuse Library objects.
|
ToolingSession | |
TraverseLoopBuilder |
The builder class for Traverse Loop component which assists you
to select or traverse a string of adjacent curves or edges.
|
TraverseLoopCollection |
Represents a collection of TraverseLoopbuilder
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimMoldComponentsBuilder |
Represents a builder to be used to create Mold Wizard trim mold components.
|
TrimMoldComponentsCollection |
Creates a TrimMoldComponentsCollection class
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimRegionBuilder |
Mold Wizard trim region management builder, trims a body to a boundary of edges, curves or bodies.
|
TrimRegionCollection |
Represents a collection of Trim Region
To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
TrimSolidBuilder |
Mold Wizard trim solid management builder, trims bounding box body with region, subtract
bounding box with workpiece or keep region and box.
|
TrimSolidCollection |
Represents a collection of Trim Solid
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
UndersizeCollection |
Creates a undersize builder
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
UnfoldingSimulationBuilder |
Unfolding Simulation Builder of PDW and EDW.
|
UniversalUnformBuilder |
Represents a
UniversalUnformBuilder builder. |
UnusedFileManagementBuilder |
Represents a
UnusedFileManagementBuilder
Unused File Management is to manage the unused files of the project. |
UnusedFileManagementCollection |
Creates a
UnusedFileManagementCollection To obtain an instance of this class, refer to ToolingManager Created in NX7.5.0 |
ValidCheckBuilder |
This is the JA builder for static interference check
To create a new instance of this class, use ValidCheckCollection.createValidCheckBuilder() Default values. |
ValidCheckCollection |
Represents a collection of ValidCheck
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WallThicknessCheckerBuilder |
Represents a builder to be used to perform wall thickness analysis.
|
WallThicknessCheckerManager |
Represents the manager of the WallThicknessChecker builder
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WireHoleBuilder |
Represents a
WireHoleBuilder
This class is for Wire Hole Design UI
To create a new instance of this class, use WireHoleCollection.createWireHoleBuilder() Default values. |
WireHoleCollection |
Creates a
WireHoleBuilder To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
WorkflowManagementCollection |
Creates a Workflow Management Collection
To obtain an instance of this class, refer to ToolingManager Created in NX8.0.0 |
WorkpieceBuilder |
Mold Wizard work piece builder
To create a new instance of this class, use WorkpieceCollection.createWorkpieceBuilder() Default values. |
WorkpieceCollection |
Creates a Workpiece Collection
To obtain an instance of this class, refer to ToolingManager Created in NX6.0.0 |
Class | Description |
---|---|
AddReusableFeatureCollection.InputData |
Defines the input data of AddReusableFeatureBuilder
|
AddReusablePart.ModeMethod |
Represents adding or editing a reusable component mode method
|
AddReusablePart.PositionMethod |
Represents the position method
|
AssemblyDrawingBuilder.AttributeNames |
Specifies the attribute name
|
AssemblyDrawingBuilder.AttributeValues |
Specifies the attribute value.
|
AssemblyDrawingBuilder.DrawingCreateOrEdit |
Specifies the sheet operation.
|
AssemblyDrawingBuilder.DrawingTypes |
Specifies the drawing type.
|
AssemblyDrawingBuilder.ModelViewToUseValue |
Specifies the model view to use.
|
AssemblyDrawingBuilder.Types |
Specifies the filter of assembly.
|
AssemblyDrawingBuilder.ViewOptionValue |
Specifies the view options.
|
AssignPatchBuilder.PatchColorData |
This class holds the data returned from
AssignPatchBuilder.getPatchColor() |
AutoDimensionBuilder.MainType |
create or edit ordinate dimension
|
AutoDimensionBuilder.TextFontType |
text font type
|
AutoDimensionBuilder.TextOrientationType |
text orientation type
|
AutoDimensionBuilder.ToleranceType |
tolerance type
|
AutoDimensionBuilder.ValuePrecisionType |
value precision type
|
BackingPadBuilder.Types |
types of backing pad design
|
BendInsertDesignBuilder.BendingDirectionOption |
the bending direction.
|
BendInsertDesignBuilder.BendTypeOption |
the bend type.
|
BendInsertDesignBuilder.BlankPositions |
Specifies the blank position.
|
BendInsertDesignBuilder.InsertTypeOption |
the insert type.
|
BendInsertDesignBuilder.ParentOption |
the parent node.
|
BendInsertDesignBuilder.Types |
the bending operation.
|
BendOperationBuilder.OverbendOptions |
The overbend option.
|
BendOperationBuilder.Prebend |
The number of children bends of prebend.
|
BendOperationBuilder.Types |
unbend operations.
|
BlankGeneratorBuilder.CreateBlankType |
Specify the creation method.
|
BlankGeneratorBuilder.EditBlankType |
Specify the edit method.
|
BlankGeneratorBuilder.Types |
Specifies the option of blank generator operation type.
|
BlankLayoutBuilder.LeftRightSideOption |
Specifies the option of left right side type.
|
BlankLayoutBuilder.SideWebOption |
Specifies the option of side webs type.
|
BlankLayoutBuilder.SnapSizeOption |
Specifies the option of snap size.
|
BlankLayoutBuilder.Types |
Specifies the option of blank layout type.
|
BlankNestingBuilder.LayoutTypeSpecification |
Specifies the layout type of blank nesting.
|
BlendCurve3DBuilder.BlendCurveOptions |
The blend curve creation methods: Best Fit, Variable, Vector, Current View
|
BlendCurve3DBuilder.InputCurvesOption |
The input curves option to keep, hide or delete input curves
|
BomBuilder.Circle |
Represents an index to the base circle type of cylinder shape.
|
BomBuilder.Shape |
Represents an index to the shape of stock size.
|
BomBuilder.TreeList |
Represents an index to components list type.
|
BomListBuilder.BomListTypes |
Represents an index to components list type.
|
BurringInsertBuilder.BurringDirections |
Specifies the burring direction.
|
BurringInsertBuilder.BurringPunchTypes |
Specifies the burring punch type.
|
BurringInsertBuilder.CircularOrNonCircularType |
Specifies the circular or non-circular type.
|
BurringInsertBuilder.DesignOptions |
Specifies the design type.
|
BurringInsertBuilder.ParentTypes |
Specifies the parent part type.
|
ChangeoverManagementBuilder.Types |
Specifies the types of changeover management.
|
ChannelAdjustBuilder.AdjustType |
the adjust method.
|
ChannelAdjustBuilder.VectorMethod |
the vector adjust method.
|
ClearanceManagementBuilder.Selection |
Specifies clearance management part.
|
ClearanceManagementBuilder.Type |
Specifies type to assign or check clearances
|
CompDrawingBuilder.ComponentTypeSelection |
Specifies the type of components.
|
CompDrawingBuilder.DrawingType |
Specifies the drawing type.
|
CompDrawingBuilder.FilterSelection |
Specifies the filter of components.
|
CompDrawingBuilder.ProjectionType |
Specifies the project type.
|
ConcurrentDesignManagementBuilder.Types |
Specifies the types of concurrent design management.
|
ConcurrentDesignManagementBuilder.UpdateTypes |
Specifies the types of the update action.
|
CoolingDefineChannelBuilder.ExtensionTypes |
The extension types of channel
|
CoolingDefineChannelBuilder.TipEndTypes |
The tip end types of channel
|
CoolingDefineChannelBuilder.Types |
Types to specify how to assign attributes to the created body.
|
CoolingExtendBuilder.TipEndTypes |
The tip end types of channel
|
CornerDesignBuilder.CornerTypeOpt |
the corner types
|
CornerDesignBuilder.SelectFromOpt |
the object selection options.
|
CornerDesignBuilder.Types |
The corner design type.
|
CreateBoxBuilder.BoxType |
the type for creating box
|
DefineCamBuilder.Types |
Specifies the cam types
|
DefineLifterBuilder.Types |
Specifies the lifter types
|
DefineNeutralFactorBuilder.FormulaOptions |
Specifies the formula used to calculate the neutral factor value
|
DieBaseBuilder.AlongDirectionOpt |
along direction options.
|
DieBaseBuilder.CatalogOpt |
catalog options.
|
DieBaseBuilder.DesignToolOption |
design tool options.
|
DieBaseBuilder.DieBaseTypeOpt |
die bse types options.
|
DieBaseBuilder.ParentNodeOpt |
parent node options.
|
DieBaseBuilder.PlatesNumberOpt |
plates number options.
|
DieBaseBuilder.SplitMethod |
split method.
|
DieBaseBuilder.Types |
die base types.
|
DieDesPierceInsertBuilder.Direction |
Represents the thickness direction.
|
DieDesPierceInsertBuilder.HoleShapeTypes |
Represents the hole shape type.
|
DieEngProcessUpdateManagerBuilder.Types |
the trim task or pierce task.
|
DieEngStampingOutputBuilder.DisplayProductType |
Types of product display.
|
DieEngStampingOutputBuilder.SpringbackMethodType |
Types of springback method
|
DieEngTrimAngleCheckBuilder.DirectionOptions |
Options to determine the method to specify direction.
|
DieEngTrimTaskBuilder.TrimTaskCamType |
the trim task cam type.
|
DieEngTrimTaskBuilder.TrimTaskMatchCutType |
the trim task match cut type.
|
DirectUnbendBuilder.Bendtypes |
unbend operations.
|
DirectUnfoldBuilder.Bend |
The number of children bends in defining prebend.
|
DirectUnfoldBuilder.BodyList |
The name list of bodies in current part.
|
DirectUnfoldBuilder.MatType |
The material database defined in PDW.
|
DirectUnfoldBuilder.Types |
Specifies the option of direct unfold type
|
EdgePatchBuilder.BodyColorData |
This class holds the data returned from
EdgePatchBuilder.getBodyColor() |
EdgePatchBuilder.PatchStatus |
Settings of the patch status types.
|
EdgePatchBuilder.SelectTypes |
Settings of the selection types.
|
EjectorPostProcessingBuilder.TrimMethod |
The processing type: Trim, Adjust length and Untrim.
|
EjectorPostProcessingBuilder.TrimPartName |
The trim part where to find a trim surface as tool to trim ejector pins.
|
EjectorPostProcessingBuilder.TrimSufaceName |
The trim surface types.
|
ElectrodeBlankBuilder.BlankMaterial |
Represents the blank material option.
|
ElectrodeBlankBuilder.BlankShape |
Represents the electrode blank shape option.
|
ElectrodeBlankBuilder.JointObject |
Represents the transition type between head bodies and the blank.
|
ElectrodeComponentBuilder.Chuck |
Represents the electrode chuck type.
|
ElectrodeCopyBuilder.Copy |
Represents an index to copy type
|
ElectrodeDeleteBuilder.Types |
delete sparking solid from blank or delete blank, pallet or holder directly.
|
EnlargeSurfaceBuilder.ColorValueData |
This class holds the data returned from
EnlargeSurfaceBuilder.getColorValue() |
EnlargeSurfaceBuilder.KeepDiscardOption |
represents the keep discard options for selected region.
|
EWDraftingBuilder.CNCTemplateOption |
the template option of cnc sheet type
|
EWDraftingBuilder.DrawingOption |
the drawing type
|
EWDraftingBuilder.EDMTemplateOption |
the template option of edm sheet type
|
EWDraftingBuilder.ModeOption |
the drafting mode option
|
EWDraftingBuilder.NameOption |
the drawing sheet name option
|
FaceColorManagementBuilder.HoleTypeEnumValue |
the hole type enumeration
|
FaceSplitBuilder.FaceSplitType |
the type for Split Face
|
FastenerAssy.HoleOperation |
Represents the action on the hole menu of the fastener assembly.
|
FastenerAssy.ModeMethod |
Represents adding and editing modes for the fastener assembly
|
FastenerAssy.SelectionObjectMethod |
Represents selection object type
|
FastenerAssy.SelectionTypeMethod |
Represents selection type for position and hole
|
FastenerAssy.StackTypeMethod |
Represents screw_array type
|
FlowDisplayBuilder.AnalysisResults |
The option of analysis results.
|
ForceCalculationBuilder.CalculationTypes |
The calculation type.
|
ForceCalculationBuilder.ProcessTypes |
The process type.
|
FormingInsertBuilder.BlankPositions |
Specifies the blank position.
|
FormingInsertBuilder.BlankTypes |
Specifies the blank type.
|
FormingInsertBuilder.DesignOptions |
Specifies the design type.
|
FormingInsertBuilder.ParentTypes |
Specifies the parent part type.
|
GeneralInsertBuilder.GenerateMethod |
Specify the creation method of insert.
|
GeneralInsertBuilder.ParentOption |
Specify the part parent of insert part.
|
GeneralInsertBuilder.Types |
Specify the insert operation type.
|
GuidedExtensionBuilder.SegmentType |
Segment type for segments
|
HoleManufacturingNoteBuilder.DefineByViewOrHoles |
the view selection or window selection type
|
HoleManufacturingNoteBuilder.HoleIndexType |
the hole index type
|
InitProjBuilder.ProjTempOption |
Represents the project template option of InitProj,
defines the pre-defined project template. this template will be used as the basic assembly structure for this new project
|
InitProjectBuilder.ConfigurationId |
the configuration type includes default and orig
|
InitProjectBuilder.MaterialId |
the material type includes None and Nylon
|
InitProjectBuilder.UnitId |
the unit type includes metric and inch project type
|
InsertAuxiliaryBuilder.CircOperationTypes |
Specifies the options of circular array.
|
InsertAuxiliaryBuilder.DesignToolOption |
Specifies the design tool option.
|
InsertAuxiliaryBuilder.RectOperationOption |
Specifies the rectangular array option.
|
InsertAuxiliaryBuilder.ShankShapeTypes |
Specifies the shank shape.
|
InsertAuxiliaryBuilder.Types |
Specifies the insert auxiliary type.
|
IntermediateStageBuilder.DesignSequences |
The types of design sequences
|
IntermediateStageBuilder.EditOptions |
The types of changed intermediate stages
|
IntermediateStageBuilder.Orientations |
The types of orientation of intermediate stages
|
LayoutBuilder.BalNumber |
Represents the number of balance cavity.
|
LayoutBuilder.LayoutSubType |
Represents the the sub type of layout.
|
LayoutBuilder.LayoutType |
Represents the type of layout.
|
LayoutBuilder.XrefNum |
Represents the type of x move refer.
|
LayoutBuilder.YrefNum |
Represents the type of y move refer.
|
LayoutManagementBuilder.StationItems |
Specifies the station items
|
LayoutRepositionBuilder.Method |
Represents the type of layout transform.
|
LayoutRepositionBuilder.Type |
Represents the method of layout transform.
|
LsdynaFormAnalysisResultDisplayBuilder.FormabilityStrainTypeName |
Options to set strain type to display for formability analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StrainTypeName |
Options to set strain type to display for strain analysis result.
|
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
Options to set stress type to display for stress analysis result.
|
LsdynaGeometryPreparationBuilder.BlankOption |
the enum of blank option.
|
LsdynaGeometryPreparationBuilder.BlankPosition |
the enum of blank position.
|
LsdynaGeometryPreparationBuilder.ContactType |
the enum of contact type.
|
LsdynaGeometryPreparationBuilder.DrawBeadType |
the enum of draw bead type.
|
LsdynaGeometryPreparationBuilder.DrawType |
the enum of draw type.
|
LsdynaGeometryPreparationBuilder.MaterialType |
the enum of material type.
|
LsdynaGeometryPreparationBuilder.ProcessActionBinder |
the enum of process action binder type.
|
LsdynaGeometryPreparationBuilder.ProcessActionDie |
the enum of process action die type.
|
LsdynaGeometryPreparationBuilder.ProcessActionPunch |
the enum of process action punch type.
|
LsdynaGeometryPreparationBuilder.ProcessType |
the enum of process type.
|
LsdynaGeometryPreparationBuilder.TargetBinder |
the enum of target binder type.
|
LsdynaGeometryPreparationBuilder.TargetDie |
the enum of target die type.
|
LsdynaGeometryPreparationBuilder.TargetPunch |
the enum of target punch type.
|
LsdynaKfileGeneratorBuilder.MeshDataType |
Types of data format.
|
LsdynaKfileGeneratorBuilder.MeshElementType |
Types of mesh element type.
|
LsdynaKfileGeneratorBuilder.OperTypes |
Types of operation.
|
MoldCsysBuilder.Wcsposition |
Represents the method to computer the WCS positino
|
MoldInsertBuilder.BooleanType |
design type: unite single workpieces, subtract overall workpieces
|
MotionSimulationBuilder.CamDefinitionType |
Specifies the way to define cam, automatically or manually.
|
MotionSimulationBuilder.EjectorMoveOptions |
Specifies the ejector move type, after or while
|
MotionSimulationBuilder.MoldbaseStyleType |
Specifies the style type of moldbase, two-plate style or three-plate style
|
MotionSimulationBuilder.Types |
Specifies the operation options of motion simulation.
|
MWCopySheetsBuilder.Types |
This enum represents the type of sheets to be copied
|
MWDefineRegionsBuilder.OrCreateEmptyRegionData |
This class holds the data returned from
MWDefineRegionsBuilder.getOrCreateEmptyRegion() |
MWDefineRegionsBuilder.TranslucencyOptionType |
This enum represents the translucency is to be performed on the selected or non-selected region faces
|
MWDesignGuideLinesBuilder.CreateGuideLineData |
This class holds the data returned from
MWDesignGuideLinesBuilder.createGuideLine(nxopen.Curve, nxopen.Point3d, double) |
MWDesignGuideLinesBuilder.DirectionType |
The type of direction for the guide line to be created.
|
MWDesignPartingSurfaceBuilder.ObjectType |
The type of parting objects to be edited or placed.
|
MWDesignPartingSurfaceBuilder.PartingSurfaceType |
The type of parting surface to be created.
|
MWDesignPartingSurfaceBuilder.TransitionSurfaceType |
The type of transition surface to be created.
|
MWDesignPartingSurfaceBuilder.TrimAndExtendFromRegionType |
The region type from which to trim and extend when creating parting surface.
|
MWMoldedPartValidationBuilder.AssignToRegion |
Options for assigning faces to the Cavity or Core region
|
MWMoldedPartValidationBuilder.CalculateOption |
Calculation options
|
MWMoldedPartValidationBuilder.CheckScope |
Check scope for information
|
MWMoldedPartValidationBuilder.RangeType |
Range type for displaying small corner radius faces
|
MWPartingManagerBuilder.DataStatus |
The status of the parting manager data.
|
MWPartingManagerBuilder.RegisterType |
The type of registering UNDO identifier.
|
ObjectAttributeManagementBuilder.FilterAccordingToAttributeType |
the selection filter type according to attribute
|
ObjectAttributeManagementBuilder.FilterType |
the selection filter type
|
ObjectAttributeManagementBuilder.ShowComponentsType |
the show type according to attribute
|
ObjectAttributeManagementBuilder.ShowType |
show attributes of selected objects or show objects according to attribute
|
PiercingInsertBuilder.AssociationToolType |
Specifies the association tool operation option.
|
PiercingInsertBuilder.DieInsertTypeItems |
Specifies the type of insert.
|
PiercingInsertBuilder.InsertPosition |
Specifies the position of piercing inserts, for EDW only
|
PiercingInsertBuilder.NormalBbpslugType |
Specifies the type of bottom plate slug.
|
PiercingInsertBuilder.NormalCavityType |
Specifies the type of cavity.
|
PiercingInsertBuilder.NormalClearanceOptionType |
Specifies the design option of piercing insert.
|
PiercingInsertBuilder.NormalDsslugType |
Specifies the type of die shoe slug.
|
PiercingInsertBuilder.NormalOffsetSideType |
Specifies the offset side of normal pierce insert design.
|
PiercingInsertBuilder.NormalUdpparentPartType |
Specifies the parent part of user defined punch.
|
PiercingInsertBuilder.PunchPocketTypeItemsBP |
Specifies the punch pocket type in backing plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsPP |
Specifies the punch pocket type in punch plate.
|
PiercingInsertBuilder.PunchPocketTypeItemsSP |
Specifies the punch pocket type in stripper plate.
|
PiercingInsertBuilder.Types |
Specifies the option of piercing insert type.
|
PocketBuilder.ModeType |
Represents the pocket operation method
|
PocketBuilder.RsetType |
Represents the pocket refset types
|
PocketBuilder.ToolType |
Represents the select type of tool
|
PrebendBuilder.NumberBendsOption |
The option of bend number to divide into
|
QuickQuotationBuilder.DesignTypes |
Specify the design type.
|
QuickQuotationBuilder.InsertGroupMaterials |
Specify the insert group material.
|
QuickQuotationBuilder.ManageTemporaryObjectsTypes |
Specify the management type for the temporary objects.
|
QuickQuotationBuilder.ObjectTypes |
Specify the concept sheet body type.
|
QuickQuotationBuilder.Types |
Specify the operation type.
|
ReliefDesignBuilder.Method |
The relief design creation method.
|
ReliefDesignBuilder.MethodOfDelete |
The relief design delete method.
|
ReliefDesignBuilder.Types |
The relief design type.
|
RemoveHolesBuilder.SelectionTypes |
select object types, body or face
|
ReusableObjectPasteBuilder.PasteMethods |
Specifies the design option
|
ReusablePocketBuilder.Hole |
Represents hole types.
|
RunnerBuilder.GuideEndType |
Represents the runner guide end type.
|
RunnerBuilder.SectionType |
Represents the section type of runner channel.
|
ScrapDesignBuilder.AddonType |
Specifies the add-on type
|
ScrapDesignBuilder.Body |
Specifies the operation type of scraps
|
ScrapDesignBuilder.DefScrapType |
Specifies the definition type of scraps
|
ScrapDesignBuilder.EditScrapType |
Specifies the edit type of scraps
|
ScrapDesignBuilder.OvercutType |
Specifies the over cut type, different type has different parameters
|
ScrapDesignBuilder.RemoveType |
Specifies the removing type as filter
|
ScrapDesignBuilder.ScrapDefPosition |
Specifies the position method of scraps, projecting method is normally used
|
ScrapDesignBuilder.ScrapDefType |
Specifies the creation type of scraps
|
ScrapDesignBuilder.TrimNumType |
Specifies the step of trimming process, the maximum is five
|
ShimBuilder.ParentOption |
Specify the parent node.
|
ShimBuilder.Types |
Specify the shim operation type.
|
SolidPatchBuilder.SolidPatchType |
Settings of the solid patch creation types.
|
SpecifyBaffleBuilder.AttributeTypes |
Types to specify how to assign attributes to the selected body.
|
SpecifyBaffleBuilder.ChannelColorData |
This class holds the data returned from
SpecifyBaffleBuilder.getChannelColor() |
SplitSolidBuilder.OperationType |
the split operation type: split, trim.
|
SplitSolidBuilder.ToolObjectOption |
the split tool selection type: Existing Object, New Plane.
|
SpreadsheetData.DefinedAttributesExpressionsData |
This class holds the data returned from
SpreadsheetData.getDefinedAttributesExpressions(nxopen.tooling.SpreadsheetData.KeywordType) |
SpreadsheetData.KeywordType |
Represents the different attribute or expression section in spreadsheet
|
SpreadsheetData.ParameterStatus |
Represents the different spreadsheet parameter status
|
SpreadsheetDataParameter.Status |
Represents the different spreadsheet parameter status
|
StandardPartBuilder.EditType |
Represents the type to edit a standard part.
|
StandardPartBuilder.RefsetName |
Represents the reference set of the standard part when it is added to the assembly.
|
StripLayoutBuilder.FromStationType |
Specifies the option of From Station for layout
|
StripLayoutBuilder.ToStationType |
Specifies the option of To Station for layout
|
SubInsertBuilder.Shape |
Represents the foot shape
|
SubInsertBuilder.Types |
Represents the type of parent part
|
ToolingApplication |
Wizard type, some of them should be same as in mpdwshare_uf_mold.h
|
ToolingCloneaction |
Clone action type
|
ToolingClonemethod |
Clone method
|
ToolingCloneparttype |
Part file type, .sim, .fem etc.
|
TraverseLoopBuilder.CheckGapData |
This class holds the data returned from
TraverseLoopBuilder.checkGap(nxopen.NXObject[]) |
TrimMoldComponentsBuilder.TargetScope |
the target bodies selection scope
|
TrimMoldComponentsBuilder.TrimMethod |
the processing type of Trim Mold Components.
|
TrimMoldComponentsBuilder.TrimPartName |
the trim part options where a part chosen to work around
|
TrimMoldComponentsBuilder.TrimSurfaceName |
trim surface types
|
TrimRegionBuilder.BoundaryOption |
represents the boundary type option, body/curve type or traverse type.
|
TrimRegionBuilder.ColorValueData |
This class holds the data returned from
TrimRegionBuilder.getColorValue() |
TrimRegionBuilder.RegionOption |
represents the option to keep or discard the selected region.
|
TrimSolidBuilder.TrimSolidAction |
represents the action to create trim solid.
|
TrimSolidBuilder.Types |
represents the option to select face or sheet body or manufacturing faces to trim the bounding box.
|
UniversalUnformBuilder.BendTypes |
The types of bend
|
UnusedFileManagementBuilder.FileDirectory |
the unused file location.
|
ValidCheckBuilder.AnalysisMode |
the analysis mode, including solid-based mode and facet-based mode
|
ValidCheckBuilder.CheckingType |
the checking type, including true body, false body or both
|
ValidCheckBuilder.SelMode |
the selection type, including component and solid body
|
WallThicknessCheckerBuilder.CalculateMethod |
The calculation method used for the wall thickness analysis.
|
WallThicknessCheckerBuilder.LegendControl |
The legend control used in displaying the thickness results.
|
WallThicknessCheckerBuilder.RangeType |
The range type for defining the ranges used in displaying the thickness results.
|
WorkpieceBuilder.MethodType |
the unit type includes the work piece define method
|
WorkpieceBuilder.Types |
the unit type includes product and combined work piece type
|
WorkpieceBuilder.WorkPieceType |
the unit type includes the work piece create method
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.