Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.ALIGNED |
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.HORIZONTAL |
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.PERPENDICULAR |
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.TEXT_AT_ANGLE |
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.TEXT_OVER_DIMENSION_LINE |
Modifier and Type | Method and Description |
---|---|
AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.textOrientation()
Returns the text orientation
License requirements: None. |
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AutoDimensionBuilder.TextOrientationType |
AutoDimensionBuilder.TextOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AutoDimensionBuilder.TextOrientationType[] |
AutoDimensionBuilder.TextOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AutoDimensionBuilder.setTextOrientation(AutoDimensionBuilder.TextOrientationType textOrientation)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.