Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.ONE_UP
Auto-position blank along x-axis without bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.PARALLELOGRAM
Auto-position blank along x-axis with parallelogram bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.RECTANGLE
Auto-position blank along x-axis with rectangle bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.TRAPEZOID
Rotate blank 180 degrees and auto-position it along x-axis with trapezoid bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.TWO_PAIR
Two pair without bounding box.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.TWO_UP
Two up without bounding box.
|
Modifier and Type | Method and Description |
---|---|
BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.layoutType()
Returns the type of layout to use in the blank nesting processing.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BlankNestingBuilder.LayoutTypeSpecification |
BlankNestingBuilder.LayoutTypeSpecification.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BlankNestingBuilder.LayoutTypeSpecification[] |
BlankNestingBuilder.LayoutTypeSpecification.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BlankNestingBuilder.setLayoutType(BlankNestingBuilder.LayoutTypeSpecification layoutType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.