Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ChannelAdjustBuilder.AdjustType |
ChannelAdjustBuilder.AdjustType.BAFFLE_LENGTH
Change the length of the baffles.
|
static ChannelAdjustBuilder.AdjustType |
ChannelAdjustBuilder.AdjustType.DISTANCE
Reposition the target channels.
|
Modifier and Type | Method and Description |
---|---|
ChannelAdjustBuilder.AdjustType |
ChannelAdjustBuilder.adjustMethod()
Returns the method for adjusting the cooling channels.
|
static ChannelAdjustBuilder.AdjustType |
ChannelAdjustBuilder.AdjustType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChannelAdjustBuilder.AdjustType |
ChannelAdjustBuilder.AdjustType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChannelAdjustBuilder.AdjustType[] |
ChannelAdjustBuilder.AdjustType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ChannelAdjustBuilder.setAdjustMethod(ChannelAdjustBuilder.AdjustType adjustMethod)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.