Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PiercingInsertBuilder.InsertPosition |
PiercingInsertBuilder.InsertPosition.BOTTOM
The position is bottom side
|
static PiercingInsertBuilder.InsertPosition |
PiercingInsertBuilder.InsertPosition.TOP
The position is top side
|
Modifier and Type | Method and Description |
---|---|
PiercingInsertBuilder.InsertPosition |
PiercingInsertBuilder.position()
Returns the reverse direction
License requirements: None. |
static PiercingInsertBuilder.InsertPosition |
PiercingInsertBuilder.InsertPosition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.InsertPosition |
PiercingInsertBuilder.InsertPosition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.InsertPosition[] |
PiercingInsertBuilder.InsertPosition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PiercingInsertBuilder.setPosition(PiercingInsertBuilder.InsertPosition position)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.