Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName.MAXIMUM_INPLANE_STRESS
Display maximum in-plane stress.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName.MINIMUM_INPLANE_STRESS
Display minimum in-plane stress.
|
Modifier and Type | Method and Description |
---|---|
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
LsdynaFormAnalysisResultDisplayBuilder.stressType()
Returns the stress type
License requirements: None. |
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName |
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaFormAnalysisResultDisplayBuilder.StressTypeName[] |
LsdynaFormAnalysisResultDisplayBuilder.StressTypeName.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaFormAnalysisResultDisplayBuilder.setStressType(LsdynaFormAnalysisResultDisplayBuilder.StressTypeName stressType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.