Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.TargetPunch.BINDER
For the process, the target of punch is binder.
|
static LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.TargetPunch.DIE
For the process, the target of punch is die.
|
static LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.TargetPunch.PUNCH
For the process, the target of punch is punch.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.targetPunchType()
Returns the type of punch target.
|
static LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.TargetPunch.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.TargetPunch |
LsdynaGeometryPreparationBuilder.TargetPunch.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.TargetPunch[] |
LsdynaGeometryPreparationBuilder.TargetPunch.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setTargetPunchType(LsdynaGeometryPreparationBuilder.TargetPunch enumTargetPunch)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.