Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ValidCheckBuilder.AnalysisMode |
ValidCheckBuilder.AnalysisMode.FACET_BASED
Facet body will be used to do checking
|
static ValidCheckBuilder.AnalysisMode |
ValidCheckBuilder.AnalysisMode.SOLID_BASED
Solid body will be used to do checking
|
Modifier and Type | Method and Description |
---|---|
ValidCheckBuilder.AnalysisMode |
ValidCheckBuilder.analyMode()
Returns the analysis mode
License requirements: None. |
static ValidCheckBuilder.AnalysisMode |
ValidCheckBuilder.AnalysisMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ValidCheckBuilder.AnalysisMode |
ValidCheckBuilder.AnalysisMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ValidCheckBuilder.AnalysisMode[] |
ValidCheckBuilder.AnalysisMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ValidCheckBuilder.setAnalyMode(ValidCheckBuilder.AnalysisMode analyMode)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.