Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.BLANK_BOUNDARY_SKETCH
Boundary curves or sketch will be used to create scraps
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.BOUNDARY_LINES
Boundary lines will be used to create an entire scrap
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.CHANGE_TYPE
The type of scrap will be changed between Piercing and Piloting
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.CLOSED_CURVES
Close curves will be used to create scraps
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.EXISTED_SHEET_BODY
Existed sheet body will be converted to scrap
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.HOLE_BOUNDARY
Hole boundary curves will be extracted automatically to create scraps
|
Modifier and Type | Method and Description |
---|---|
ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.scrapMethod()
Returns the scrap method, which includes boundary+sketch, hole boundary, close curves, boundary lines and existed sheet body
License requirements: None. |
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ScrapDesignBuilder.ScrapDefType |
ScrapDesignBuilder.ScrapDefType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ScrapDesignBuilder.ScrapDefType[] |
ScrapDesignBuilder.ScrapDefType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ScrapDesignBuilder.setScrapMethod(ScrapDesignBuilder.ScrapDefType scrapMethod)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.