Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.AssociationToolType.ADD_INTO_LIST
The operation option is add into list
|
static PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.AssociationToolType.DELETE_SELECTED_INSERTS
The operation option is delete selected inserts
|
static PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.AssociationToolType.REMOVE_FROM_LIST
The operation option is remove from list
|
Modifier and Type | Method and Description |
---|---|
PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.associationTool()
Returns the association tool type.
|
static PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.AssociationToolType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.AssociationToolType |
PiercingInsertBuilder.AssociationToolType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.AssociationToolType[] |
PiercingInsertBuilder.AssociationToolType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PiercingInsertBuilder.setAssociationTool(PiercingInsertBuilder.AssociationToolType associationTool)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.