Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.PLATE_EIGHT
plates number is 8
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.PLATE_FIVE
plates number is 5
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.PLATE_NINE
plates number is 9
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.PLATE_TEN
plates number is 10
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.PLATE_TWELVE
plates number is 12
|
Modifier and Type | Method and Description |
---|---|
DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.platesNumber()
Returns the user defined plates number.
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBaseBuilder.PlatesNumberOpt |
DieBaseBuilder.PlatesNumberOpt.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBaseBuilder.PlatesNumberOpt[] |
DieBaseBuilder.PlatesNumberOpt.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieBaseBuilder.setPlatesNumber(DieBaseBuilder.PlatesNumberOpt platesNumber)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") OR nx_engineering_die_wizard ("NX Engineering Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.