Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.TargetDie.BINDER
For the process, the target of die is binder.
|
static LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.TargetDie.DIE
For the process, the target of die is die.
|
static LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.TargetDie.PUNCH
For the process, the target of die is punch.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.targetDieType()
Returns the type of die target.
|
static LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.TargetDie.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.TargetDie |
LsdynaGeometryPreparationBuilder.TargetDie.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.TargetDie[] |
LsdynaGeometryPreparationBuilder.TargetDie.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setTargetDieType(LsdynaGeometryPreparationBuilder.TargetDie enumTargetDie)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.