Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaKfileGeneratorBuilder.OperTypes |
LsdynaKfileGeneratorBuilder.OperTypes.MESH
Meshes the forming object
|
static LsdynaKfileGeneratorBuilder.OperTypes |
LsdynaKfileGeneratorBuilder.OperTypes.RUNSOLVER
Runs LS-DYNA solver
|
Modifier and Type | Method and Description |
---|---|
LsdynaKfileGeneratorBuilder.OperTypes |
LsdynaKfileGeneratorBuilder.type()
Returns the type of operation to be run.
|
static LsdynaKfileGeneratorBuilder.OperTypes |
LsdynaKfileGeneratorBuilder.OperTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaKfileGeneratorBuilder.OperTypes |
LsdynaKfileGeneratorBuilder.OperTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaKfileGeneratorBuilder.OperTypes[] |
LsdynaKfileGeneratorBuilder.OperTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaKfileGeneratorBuilder.setType(LsdynaKfileGeneratorBuilder.OperTypes type)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.