Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaGeometryPreparationBuilder.BlankPosition |
LsdynaGeometryPreparationBuilder.BlankPosition.ABOVE_BINDER
Blank sheet body is above binder.
|
static LsdynaGeometryPreparationBuilder.BlankPosition |
LsdynaGeometryPreparationBuilder.BlankPosition.ABOVE_BINDERAND_PUNCH
Blank sheet body is above binder and punch.
|
Modifier and Type | Method and Description |
---|---|
LsdynaGeometryPreparationBuilder.BlankPosition |
LsdynaGeometryPreparationBuilder.blankPositionType()
Returns the blank position type.
|
static LsdynaGeometryPreparationBuilder.BlankPosition |
LsdynaGeometryPreparationBuilder.BlankPosition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaGeometryPreparationBuilder.BlankPosition |
LsdynaGeometryPreparationBuilder.BlankPosition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaGeometryPreparationBuilder.BlankPosition[] |
LsdynaGeometryPreparationBuilder.BlankPosition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaGeometryPreparationBuilder.setBlankPositionType(LsdynaGeometryPreparationBuilder.BlankPosition enumBlankPosition)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.