Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static StandardPartBuilder.EditType |
StandardPartBuilder.EditType.ADD_INSTANCE |
static StandardPartBuilder.EditType |
StandardPartBuilder.EditType.MODIFY |
static StandardPartBuilder.EditType |
StandardPartBuilder.EditType.NEW_COMPONENT |
Modifier and Type | Method and Description |
---|---|
StandardPartBuilder.EditType |
StandardPartBuilder.standardPartEditType()
Returns the standard part edit type of processing the selected component.
|
static StandardPartBuilder.EditType |
StandardPartBuilder.EditType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StandardPartBuilder.EditType |
StandardPartBuilder.EditType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StandardPartBuilder.EditType[] |
StandardPartBuilder.EditType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StandardPartBuilder.setStandardPartEditType(StandardPartBuilder.EditType standardPartEditType)
License requirements: ug_mold_design ("UG MOLD") OR nx_electrode_wizard ("NX Electrode Wizard") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.