Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static TrimRegionBuilder.RegionOption |
TrimRegionBuilder.RegionOption.DISCARD
selected region will be discarded.
|
static TrimRegionBuilder.RegionOption |
TrimRegionBuilder.RegionOption.KEEP
selected region will be kept.
|
Modifier and Type | Method and Description |
---|---|
TrimRegionBuilder.RegionOption |
TrimRegionBuilder.regionType()
Returns the value of the option, which specifies to keep or discard the selected region.
|
static TrimRegionBuilder.RegionOption |
TrimRegionBuilder.RegionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimRegionBuilder.RegionOption |
TrimRegionBuilder.RegionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimRegionBuilder.RegionOption[] |
TrimRegionBuilder.RegionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimRegionBuilder.setRegionType(TrimRegionBuilder.RegionOption regionType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.