Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static QuickQuotationBuilder.InsertGroupMaterials |
QuickQuotationBuilder.InsertGroupMaterials.CR12
insert group material is Cr12
|
static QuickQuotationBuilder.InsertGroupMaterials |
QuickQuotationBuilder.InsertGroupMaterials.CR12MO_V
insert group material is Cr12MoV
|
Modifier and Type | Method and Description |
---|---|
QuickQuotationBuilder.InsertGroupMaterials |
QuickQuotationBuilder.insertGroupMaterial()
Returns the insert group material.
|
static QuickQuotationBuilder.InsertGroupMaterials |
QuickQuotationBuilder.InsertGroupMaterials.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static QuickQuotationBuilder.InsertGroupMaterials |
QuickQuotationBuilder.InsertGroupMaterials.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static QuickQuotationBuilder.InsertGroupMaterials[] |
QuickQuotationBuilder.InsertGroupMaterials.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
QuickQuotationBuilder.setInsertGroupMaterial(QuickQuotationBuilder.InsertGroupMaterials insertGroupMaterial)
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") OR nx_engineering_die_wizard ("NX Engineering Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.