Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieDesPierceInsertBuilder.Direction |
DieDesPierceInsertBuilder.Direction.LOWER |
static DieDesPierceInsertBuilder.Direction |
DieDesPierceInsertBuilder.Direction.UPPER |
Modifier and Type | Method and Description |
---|---|
DieDesPierceInsertBuilder.Direction |
DieDesPierceInsertBuilder.thicknessDirectionOption()
Returns the thickness direction option.
|
static DieDesPierceInsertBuilder.Direction |
DieDesPierceInsertBuilder.Direction.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieDesPierceInsertBuilder.Direction |
DieDesPierceInsertBuilder.Direction.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieDesPierceInsertBuilder.Direction[] |
DieDesPierceInsertBuilder.Direction.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieDesPierceInsertBuilder.setThicknessDirectionOption(DieDesPierceInsertBuilder.Direction thicknessDirectionOption)
License requirements: ug_die_design ("Die Design") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.