Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LsdynaKfileGeneratorBuilder.MeshDataType |
LsdynaKfileGeneratorBuilder.MeshDataType.LONG_BIT
64 bit format
|
static LsdynaKfileGeneratorBuilder.MeshDataType |
LsdynaKfileGeneratorBuilder.MeshDataType.SHORT_BIT
32 bit IEEE format
|
Modifier and Type | Method and Description |
---|---|
LsdynaKfileGeneratorBuilder.MeshDataType |
LsdynaKfileGeneratorBuilder.dataType()
Returns the data type
License requirements: None. |
static LsdynaKfileGeneratorBuilder.MeshDataType |
LsdynaKfileGeneratorBuilder.MeshDataType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LsdynaKfileGeneratorBuilder.MeshDataType |
LsdynaKfileGeneratorBuilder.MeshDataType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LsdynaKfileGeneratorBuilder.MeshDataType[] |
LsdynaKfileGeneratorBuilder.MeshDataType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LsdynaKfileGeneratorBuilder.setDataType(LsdynaKfileGeneratorBuilder.MeshDataType dataType)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.