Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.PunchPocketTypeItemsBP.CIRCLE
Punch pocket type in backing plate is circle
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.PunchPocketTypeItemsBP.CLEARANCE
Punch pocket type in backing plate is clearance
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.PunchPocketTypeItemsBP.FILLET
Punch pocket type in backing plate is fillet
|
Modifier and Type | Method and Description |
---|---|
PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.punchPocketTypeInBP()
Returns the punch pocket type in backing plate.
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.PunchPocketTypeItemsBP.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP |
PiercingInsertBuilder.PunchPocketTypeItemsBP.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PiercingInsertBuilder.PunchPocketTypeItemsBP[] |
PiercingInsertBuilder.PunchPocketTypeItemsBP.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PiercingInsertBuilder.setPunchPocketTypeInBP(PiercingInsertBuilder.PunchPocketTypeItemsBP punchPocketTypeInBP)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.