Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.ADDON
Add-on operation
|
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.CREATE
Create operation
|
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.EDIT
Edit operation
|
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.GROUPING
Grouping operation
|
Modifier and Type | Method and Description |
---|---|
ScrapDesignBuilder.Body |
ScrapDesignBuilder.scrapTypeEnum()
Returns the scrap type enum
License requirements: None. |
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ScrapDesignBuilder.Body |
ScrapDesignBuilder.Body.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ScrapDesignBuilder.Body[] |
ScrapDesignBuilder.Body.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ScrapDesignBuilder.setScrapTypeEnum(ScrapDesignBuilder.Body scrapTypeEnum)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.