Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.BlankPositions.DIE_PLATE
the blank is on the die plate
|
static FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.BlankPositions.PUNCH_PLATE
the blank is on the punch plate
|
static FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.BlankPositions.STRIPPER_PLATE
the blank is on the stripper plate
|
Modifier and Type | Method and Description |
---|---|
FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.blankPosition()
Returns the blank position in punch plate or stripper plate.
|
static FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.BlankPositions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormingInsertBuilder.BlankPositions |
FormingInsertBuilder.BlankPositions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormingInsertBuilder.BlankPositions[] |
FormingInsertBuilder.BlankPositions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FormingInsertBuilder.setBlankPosition(FormingInsertBuilder.BlankPositions blankPosition)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.