Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static SubInsertBuilder.Shape |
SubInsertBuilder.Shape.BOX
The shape is a block
|
static SubInsertBuilder.Shape |
SubInsertBuilder.Shape.CYLINDER
The shape is a cylinder
|
Modifier and Type | Method and Description |
---|---|
SubInsertBuilder.Shape |
SubInsertBuilder.selFootType()
Returns the foot type which can be a box or a cylinder
License requirements: None. |
static SubInsertBuilder.Shape |
SubInsertBuilder.Shape.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubInsertBuilder.Shape |
SubInsertBuilder.Shape.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubInsertBuilder.Shape[] |
SubInsertBuilder.Shape.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubInsertBuilder.setSelFootType(SubInsertBuilder.Shape selFootType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.