Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DirectUnfoldBuilder.MatType |
DirectUnfoldBuilder.MatType.STEEL
Default is steel.
|
Modifier and Type | Method and Description |
---|---|
DirectUnfoldBuilder.MatType |
DirectUnfoldBuilder.materials()
Deprecated.
Deprecated in NX10.0.0. Use
Tooling.DefineNeutralFactorBuilder#partMaterial instead.
|
static DirectUnfoldBuilder.MatType |
DirectUnfoldBuilder.MatType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DirectUnfoldBuilder.MatType |
DirectUnfoldBuilder.MatType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DirectUnfoldBuilder.MatType[] |
DirectUnfoldBuilder.MatType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DirectUnfoldBuilder.setMaterials(DirectUnfoldBuilder.MatType materials)
Deprecated.
Deprecated in NX10.0.0. Use
Tooling.DefineNeutralFactorBuilder#setPartMaterial instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.