Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.CURVES_EDGES
using curve or edge for Split Face
|
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.INTERSECTION
using intersection curve of two body for Split Face
|
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.ISOCLINE
using Isocline for Split Face
|
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.PLANE
using plane for Split Face
|
Modifier and Type | Method and Description |
---|---|
FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.type()
Returns the split face type which splits a face by using curves, edges, plane, face, isolines or
intersected curves with another body
License requirements: None. |
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FaceSplitBuilder.FaceSplitType |
FaceSplitBuilder.FaceSplitType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FaceSplitBuilder.FaceSplitType[] |
FaceSplitBuilder.FaceSplitType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FaceSplitBuilder.setType(FaceSplitBuilder.FaceSplitType splitType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.