Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static HoleManufacturingNoteBuilder.DefineByViewOrHoles |
HoleManufacturingNoteBuilder.DefineByViewOrHoles.HOLES |
static HoleManufacturingNoteBuilder.DefineByViewOrHoles |
HoleManufacturingNoteBuilder.DefineByViewOrHoles.VIEW |
Modifier and Type | Method and Description |
---|---|
HoleManufacturingNoteBuilder.DefineByViewOrHoles |
HoleManufacturingNoteBuilder.defineByViewOrHolesEnum()
Returns the selection type enumeration
License requirements: None. |
static HoleManufacturingNoteBuilder.DefineByViewOrHoles |
HoleManufacturingNoteBuilder.DefineByViewOrHoles.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleManufacturingNoteBuilder.DefineByViewOrHoles |
HoleManufacturingNoteBuilder.DefineByViewOrHoles.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleManufacturingNoteBuilder.DefineByViewOrHoles[] |
HoleManufacturingNoteBuilder.DefineByViewOrHoles.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleManufacturingNoteBuilder.setDefineByViewOrHolesEnum(HoleManufacturingNoteBuilder.DefineByViewOrHoles defineByViewOrHoles)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.