Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static AssemblyDrawingBuilder.DrawingCreateOrEdit |
AssemblyDrawingBuilder.DrawingCreateOrEdit.CREATE_NEW |
static AssemblyDrawingBuilder.DrawingCreateOrEdit |
AssemblyDrawingBuilder.DrawingCreateOrEdit.SH1 |
Modifier and Type | Method and Description |
---|---|
AssemblyDrawingBuilder.DrawingCreateOrEdit |
AssemblyDrawingBuilder.enumSheets()
Returns the option for select the sheet
License requirements: None. |
static AssemblyDrawingBuilder.DrawingCreateOrEdit |
AssemblyDrawingBuilder.DrawingCreateOrEdit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssemblyDrawingBuilder.DrawingCreateOrEdit |
AssemblyDrawingBuilder.DrawingCreateOrEdit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssemblyDrawingBuilder.DrawingCreateOrEdit[] |
AssemblyDrawingBuilder.DrawingCreateOrEdit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssemblyDrawingBuilder.setEnumSheets(AssemblyDrawingBuilder.DrawingCreateOrEdit enumSheets)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.