Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.HoleIndexType.ALPHABETIC |
static HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.HoleIndexType.NUMERIC |
static HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.HoleIndexType.USER_DEFINED_AND_NUMBER |
Modifier and Type | Method and Description |
---|---|
HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.holeIndexTypeEnum()
Returns the hole index type enumeration
License requirements: None. |
static HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.HoleIndexType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleManufacturingNoteBuilder.HoleIndexType |
HoleManufacturingNoteBuilder.HoleIndexType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleManufacturingNoteBuilder.HoleIndexType[] |
HoleManufacturingNoteBuilder.HoleIndexType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleManufacturingNoteBuilder.setHoleIndexTypeEnum(HoleManufacturingNoteBuilder.HoleIndexType holeIndexTypeEnum)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.