Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static DieEngTrimAngleCheckBuilder.DirectionOptions |
DieEngTrimAngleCheckBuilder.DirectionOptions.BY_ANGLES |
static DieEngTrimAngleCheckBuilder.DirectionOptions |
DieEngTrimAngleCheckBuilder.DirectionOptions.BY_VECTOR |
Modifier and Type | Method and Description |
---|---|
DieEngTrimAngleCheckBuilder.DirectionOptions |
DieEngTrimAngleCheckBuilder.directionOption()
Returns the option to set the method of defining trimming direction
License requirements: None. |
static DieEngTrimAngleCheckBuilder.DirectionOptions |
DieEngTrimAngleCheckBuilder.DirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieEngTrimAngleCheckBuilder.DirectionOptions |
DieEngTrimAngleCheckBuilder.DirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieEngTrimAngleCheckBuilder.DirectionOptions[] |
DieEngTrimAngleCheckBuilder.DirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieEngTrimAngleCheckBuilder.setDirectionOption(DieEngTrimAngleCheckBuilder.DirectionOptions directionOption)
License requirements: die_engineering ("DIE ENGINEERING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.