Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.StationItems.ONE
Define station number -- 01
|
static LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.StationItems.THREE
Define station number -- 03
|
static LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.StationItems.TWO
Define station number -- 02
|
Modifier and Type | Method and Description |
---|---|
LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.stationEnum()
Returns the station number definition of engineering die
License requirements: None. |
static LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.StationItems.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LayoutManagementBuilder.StationItems |
LayoutManagementBuilder.StationItems.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LayoutManagementBuilder.StationItems[] |
LayoutManagementBuilder.StationItems.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LayoutManagementBuilder.setStationEnum(LayoutManagementBuilder.StationItems stationEnum)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.