Package | Description |
---|---|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Field and Description |
---|---|
static CompDrawingBuilder.ProjectionType |
CompDrawingBuilder.ProjectionType.FIRST_ANGLE_PROJECTION
first angle projection
|
static CompDrawingBuilder.ProjectionType |
CompDrawingBuilder.ProjectionType.THIRD_ANGLE_PROJECTION
third angle projection
|
Modifier and Type | Method and Description |
---|---|
CompDrawingBuilder.ProjectionType |
CompDrawingBuilder.projection()
Returns the drawing projection angle.
|
static CompDrawingBuilder.ProjectionType |
CompDrawingBuilder.ProjectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CompDrawingBuilder.ProjectionType |
CompDrawingBuilder.ProjectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CompDrawingBuilder.ProjectionType[] |
CompDrawingBuilder.ProjectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CompDrawingBuilder.setProjection(CompDrawingBuilder.ProjectionType projection)
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.