Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Class and Description |
---|
DieSimCollection
Represents a collection of Die Simulation - Press Models
To obtain an instance of this class, refer to Part Created in NX6.0.0 |
Class and Description |
---|
AddendumSectionBuilder
Represents a
AddendumSectionBuilder which is used to create or edit an addendum section. |
AddendumSectionBuilder.SectionLocationType
The settings indicating the location of the section being created.
|
AddendumSectionBuilder.SectionOrientationType
The settings to indicate the section orientation.
|
AddendumSectionBuilder.SectionShapeType
The settings to indicate the section shape.
|
AddendumSectionBuilder.SegmentParameterType
The settings to indicate which parameter of the segment to lock.
|
AddendumSectionBuilder.SegmentType
The settings to indicate the segment type to update.
|
AddendumSectionBuilder.SurfaceBuildType
The settings to indicate the surface type.
|
AddendumSectionUserDefinedBuilder
Represents a
AddendumSectionUserDefinedBuilder builder used to select a previously
defined section or a string of objects to define the section shape. |
AddSurfBuilder
Represents a
AddSurfBuilder builder
To create a new instance of this class, use DieCollection.createAddSurfBuilder(nxopen.features.Feature) Created in NX6.0.0 |
AddSurfBuilder.Methods
Settings for the type of addendum surface being created.
|
CastRelief
Represents a cast relief feature
To create or edit an instance of this class, use CastReliefBuilder Created in NX6.0.0 |
CastReliefBuilder
Represents a
CastReliefBuilder builder
To create a new instance of this class, use DieCollection.castRelief(nxopen.die.CastRelief) Default values. |
CastReliefParentBuilder
Represents a Die Cast Relief sub feature.
|
CastReliefParentBuilder.CastReliefData
This class holds the data returned from
CastReliefParentBuilder.getCastRelief() |
ClampingSlot
Represents a clamping slot feature
To create or edit an instance of this class, use ClampingSlotBuilder Created in NX6.0.0 |
ClampingSlotBuilder
Represents a Clamping Slot feature builder
To create a new instance of this class, use DieCollection.clampingSlot(nxopen.die.ClampingSlot) Default values. |
ClampingSlotBuilder.Types
Clamping slot types
|
Clearance
Represents a die design clearance feature.
|
ClearanceBuilder
Represents a builder that is used to create or edit a
Clearance feature. |
ClearanceBuilder.ClearanceGeometryTypes
Identifies which type of input defines the clearance.
|
ClearanceBuilder.Types
Identifies which clearance type is being created in the casting.
|
CompensateRoughDataBuilder
Represents a
CompensateRoughDataBuilder . |
CompensateRoughDataBuilder.ApproximationType
Settings for the amount of approximation to perform.
|
CompensateRoughDataBuilder.Types
Settings for the type of data being compensated.
|
ConnectProfileParentBuilder
Represents a Die Connecting Profile sub feature.
|
ConnectProfileParentBuilder.ProfileData
This class holds the data returned from
ConnectProfileParentBuilder.getProfile() |
DeckParentBuilder
Represents a Die Deck Feature sub feature.
|
DeckParentBuilder.MainDeckData
This class holds the data returned from
DeckParentBuilder.getMainDeck() |
DieAssistantFlangeProfile |
DieAssistantFlangeProfileList
Represents a list of objects.
|
DieAssistantFlangeProfileType
Settings for the flange type.
|
DieAssistantTrimProfile |
DieAssistantTrimProfileList
Represents a list of objects.
|
DieAttributesBuilder
Represents a
DieAttributesBuilder . |
DieBooleanBuilder
Represents a
DieBooleanBuilder . |
DieBooleanBuilder.BooleanType
boolean type to apply to the selected solids
|
DieBooleanBuilderList
Represents a list of objects.
|
DieBuildStatusOption
Settings for the build status of the die design sub features.
|
DieDirectionBuilder
Represents a
DieDirectionBuilder . |
DieDirectionBuilder.DirectionType
the options available for defining the direction
|
DieLimitsBuilder
Limits a path to a segment of the path.
|
DieLocationBuilder
Represents a
DieLocationBuilder . |
DieLocationBuilder.LocationType
the options available for defining the location
|
DieLocationBuilderList
Represents a list of objects.
|
DieLocationsBuilder
Represents a
DieLocationsBuilder . |
DiePlaneBuilder
Represents a
DiePlaneBuilder . |
DiePlaneBuilder.PlaneType
the options available for defining the plane
|
DieShoe
Represents a die shoe feature
To create or edit an instance of this class, use DieShoeBuilder Created in NX6.0.0 |
DieShoeBuilder
Represents a Die Shoe feature builder.
|
DirectionOption
Settings for the profile direction.
|
DrawBead
Represents a draw bead feature.
|
DrawBeadBuilder
Represents a builder that is used to create or edit a
DrawBead feature. |
DrawBeadBuilder.FemaleDepthTypes
Specifies how the female depth is calculated or defined.
|
DrawBeadBuilder.FemaleWidthTypes
Specifies how the feamle width is calcualted or defined.
|
DrawBeadBuilder.MaleBeadPositionTypes
Identifes which casting the male bead is created in.
|
DrawBeadBuilder.OrientationTypes
Identifies the orientation of the base parameters to the sheet metal.
|
DrawBeadBuilder.OrientSectionToDrawTypes
Specifies if the segment height section parameter should be oriented to the draw direction or the sheet metal normal at the section location.
|
DrawBeadBuilder.OutputTypes
Specifies what type of output is desired for the feature creation.
|
DrawBeadBuilder.ProjectionDirectionTypes
Identifes how the centerline should be projected to the placement face during processing.
|
DrawBeadBuilder.TransitionDefinitionTypes
Specifies how the transition area should be determined from segment to segment within a single bead.
|
DrawBeadSegmentBuilder
Segment builder for Die Engineering draw bead.
|
DrawBeadSegmentBuilder.MaleBeadWidthTypes
value for how the male width is specified.
|
DrawBeadSegmentBuilderList
Represents a list of objects.
|
DrawBeadTaperBuilder
Taper definition for the end of the Die Engineering Draw Bead.
|
DrawBeadTaperBuilder.TaperTypes
Taper types to define how the slope is created for the bead end.
|
DrawDiePunchBuilder
Represents a Draw Die Punch feature builder.
|
DrawDiePunchBuilder.PunchProfileData
This class holds the data returned from
DrawDiePunchBuilder.getPunchProfile() |
DrawDiePunchSectionBuilder
Represents a Draw Die Punch Section sub feature.
|
DrawDiePunchSectionBuilder.FormingAttributesData
This class holds the data returned from
DrawDiePunchSectionBuilder.getFormingAttributes() |
DrawDiePunchSectionBuilder.PunchProfileAttributesData
This class holds the data returned from
DrawDiePunchSectionBuilder.getPunchProfileAttributes() |
FaceSheetBuilder
Represents a Face Sheet feature
This is an abstract class, and cannot be created. |
FillArea
Represents a die design fill area feature.
|
FillAreaBuilder
Represents a builder that is used to create or edit a
FillArea feature. |
FillAreaBuilder.Types
Identifies the area of the casting the fill is targeted for.
|
FillAreaBuilder.UpperLimitTypes
Specifies how the upper limit of the fill area is defined.
|
FillBuilder
Represents an Area Fill feature
To create a new instance of this class, use DieCollection.fill(nxopen.features.Feature) Created in NX4.0.0 |
FillBuilder.RegionBoundsData
This class holds the data returned from
FillBuilder.getRegionBounds() |
FingerClearanceNotch
Represents a die design finger clearance notch feature.
|
FingerClearanceNotchBuilder
Represents a builder that is used to create or edit a
FingerClearanceNotch feature. |
FingerClearanceNotchBuilder.Types
Specifies what type of base geometry to build the finger clearance notch from.
|
FlangeSteelRibChildBuilder
Represents a Die Flange Steel Rib Child sub feature.
|
FlangeSteelRibParentBuilder
Represents a Die Flange Steel Rib Parent sub feature.
|
FlangeTaskBuilder
Represents a Flange Task feature builder.
|
FlangeTaskBuilder.CameraLayerAndXmlpData
This class holds the data returned from
FlangeTaskBuilder.getCameraLayerAndXmlp() |
FlangeTaskBuilder.CamTypes
Settings for the cam type of the flange task.
|
FlangeTaskBuilder.PierceTypes
Settings for the pierce type of the flange task.
|
FlangeTaskBuilder.RegionBoundsData
This class holds the data returned from
FlangeTaskBuilder.getRegionBounds() |
FlangeTaskBuilder.SpringbackTypes
Settings for the springback type of the flange task.
|
FormTaskBuilder
Represents a Form Task feature builder.
|
FormTaskBuilder.RegionBoundsData
This class holds the data returned from
FormTaskBuilder.getRegionBounds() |
HandlingCore
Represents a die design handling core feature.
|
HandlingCoreBuilder
Represents a builder that is used to create or edit a
HandlingCore feature. |
HandlingCoreBuilder.Types
Identifies how the handling Core is located in space.
|
HandlingCoreChildBuilder
Represents a Die Handling Core Child sub feature.
|
HandlingCoreParentBuilder
Represents a Die Handling Core Parent sub feature.
|
Heelpost
Represents a heelpost feature
To create or edit an instance of this class, use HeelpostBuilder Created in NX6.0.0 |
HeelpostBuilder
Represents a
HeelpostBuilder builder
To create a new instance of this class, use DieCollection.heelpost(nxopen.die.Heelpost) Default values. |
HeelpostBuilder.Types
Heelpost types
|
HoleChildBuilder
Represents a Die Hole Child sub feature.
|
HoleChildBuilder.HoleAttributesData
This class holds the data returned from
HoleChildBuilder.getHoleAttributes() |
HoleChildBuilder.PadAttributesData
This class holds the data returned from
HoleChildBuilder.getPadAttributes() |
HoleParentBuilder
Represents a Die Hole Parent sub feature.
|
HoleParentBuilder.HoleAttributesData
This class holds the data returned from
HoleParentBuilder.getHoleAttributes() |
HoleParentBuilder.PadAttributesData
This class holds the data returned from
HoleParentBuilder.getPadAttributes() |
Keyway
Represents a keyway feature
To create or edit an instance of this class, use KeywayBuilder Created in NX6.0.0 |
KeywayBuilder
Represents a
KeywayBuilder builder
To create a new instance of this class, use DieCollection.keyway(nxopen.die.Keyway) Default values. |
KeywayBuilder.LocationType
Keyway location direction relative to the die centerline coordinate system
|
KeywayBuilder.Types
Keyway runoff types
|
KeywayChildBuilder
Represents a Die Keyway Child sub feature.
|
KeywayChildBuilder.LocationOption
Settings for the location of the keyway.
|
KeywayChildBuilder.RunoffTypeOption
Settings for the runoff type of the keyway.
|
KeywayChildBuilder.SlotAttributesData
This class holds the data returned from
KeywayChildBuilder.getSlotAttributes() |
KeywayParentBuilder
Represents a Die Keyway Parent sub feature.
|
KeywayParentBuilder.RunoffTypeOption
Settings for the runoff type of the keyway.
|
KeywayParentBuilder.SlotAttributesData
This class holds the data returned from
KeywayParentBuilder.getSlotAttributes() |
LineupBuilder
Represents a Lineup feature builder
To create a new instance of this class, use DieCollection.lineup(nxopen.features.Feature) Created in NX4.0.0 |
MachineRelief
Represents a die design machine relief feature.
|
MachineReliefBuilder
Represents a builder that is used to create or edit a
MachineRelief feature. |
MachineReliefBuilder.MainProfileTypes
Specifies that the profile is for an exterior or interior profile.
|
MachineReliefBuilder.TrimSheetTypes
Specifies what the trimming surface is defined by.
|
MachineReliefBuilder.Types
Identifies the type of structure to be added, or subtracted, to the casting.
|
OutputCurvesBuilder
Represents an output curves feature builder.
|
OutputCurvesBuilder.SmoothTypes
Settings for the curve smoothing type.
|
OutputCurvesBuilder.TrimCurveCreateTypes
Settings for the trim curve creation type.
|
OutputCurvesBuilder.TrimCurveTypes
Settings for the trim curve type.
|
OutputCurvesBuilder.TrimOutputCurveTypes
Settings for the trim curve output type.
|
PadChildBuilder
Represents a Die Pad Child sub feature.
|
PadChildBuilder.HoleAttributesData
This class holds the data returned from
PadChildBuilder.getHoleAttributes() |
PadChildBuilder.PadAttributesData
This class holds the data returned from
PadChildBuilder.getPadAttributes() |
PadChildBuilder.ShapeData
This class holds the data returned from
PadChildBuilder.getShape() |
PadChildBuilder.ShapeTypeOption
Settings for the shape type of the die pad.
|
PadParentBuilder
Represents a Die Pad Parent sub feature.
|
PadParentBuilder.HoleAttributesData
This class holds the data returned from
PadParentBuilder.getHoleAttributes() |
PadParentBuilder.PadAttributesData
This class holds the data returned from
PadParentBuilder.getPadAttributes() |
PadParentBuilder.ShapeTypeOption
Settings for the shape type of the die pads.
|
PierceHoleChildBuilder
Represents a Pierce Hole Child sub feature.
|
PierceHoleChildBuilder.HoleAttributesData
This class holds the data returned from
PierceHoleChildBuilder.getHoleAttributes() |
PierceHoleChildBuilder.PierceHoleShapeData
This class holds the data returned from
PierceHoleChildBuilder.getPierceHoleShape() |
PierceHoleChildBuilder.ShapeTypeOption
Settings for the shape type of the pierce hole.
|
PierceHoleParentBuilder
Represents a Pierce Hole Parent sub feature.
|
PierceHoleParentBuilder.HoleAttributesData
This class holds the data returned from
PierceHoleParentBuilder.getHoleAttributes() |
PierceItemBuilder |
PierceItemBuilder.HoleShapeType
Settings for the hole shape of individual pierces.
|
PierceItemBuilder.SizingMethodOption
Settings for the sizing method of individual pierces.
|
PierceItemBuilderList
Represents a list of objects.
|
PierceTaskBuilder
Represents a Pierce Task feature builder
To create a new instance of this class, use DieCollection.pierceTask(nxopen.features.Feature) Created in NX4.0.0 |
PierceTaskBuilder.CameraLayerAndXmlpData
This class holds the data returned from
PierceTaskBuilder.getCameraLayerAndXmlp() |
PierceTaskBuilder.CamTypes
Settings for the cam type of the pierce task.
|
PierceTaskBuilder.CenterPointOptionTypes
Settings for the center point output options of the pierce task.
|
PierceTaskBuilder.PierceBoundsData
This class holds the data returned from
PierceTaskBuilder.getPierceBounds() |
PierceTaskBuilder.PrecisionTypes
Settings for the precistion type of the pierce task.
|
PointChildBuilder
Represents a Die Point Child sub feature.
|
PointParentBuilder
Represents a Die Point Parent sub feature.
|
PressModel
Represents a Die Simulation - Press Model .
|
PressureSystemChildBuilder
Represents a Die Pressure System Child sub feature.
|
PressureSystemParentBuilder
Represents a Die Pressure System Parent sub feature.
|
QuickBinderBuilder
Represents a
QuickBinderBuilder builder which builds a developable binder sheet
body by adding cones, cylinders, or planes to an approximated face. |
QuickBinderBuilder.EdgesOfFaceData
This class holds the data returned from
QuickBinderBuilder.getEdgesOfFace(int) |
QuickBinderBuilder.EditTypes
The type of edit to be performed on the face.
|
QuickBinderBuilder.Types
The method used to approximate the product faces.
|
QuickBinderWrapBuilder
Represents a
QuickBinderWrapBuilder builder
This is an abstract class, and cannot be created. |
QuickBinderWrapBuilder.EditSizeType
Settings for the edit size type.
|
QuickBinderWrapBuilder.Types
Settings for the binder wrap sheet body type.
|
RibChildBuilder
Represents a Die Rib Child sub feature.
|
RibChildBuilder.CenterlineData
This class holds the data returned from
RibChildBuilder.getCenterline() |
RibParentBuilder
Represents a Die Rib Parent sub feature.
|
RotorBuilder
Represents a CAM Rotor feature builder.
|
RotorBuilder.FlangeBendProfileData
This class holds the data returned from
RotorBuilder.getFlangeBendProfile() |
RotorSectionBuilder
Represents a Rotor Section sub feature.
|
RotorSectionBuilder.RotorAttributesData
This class holds the data returned from
RotorSectionBuilder.getRotorAttributes() |
SpringbackCompensation
Represents a springback compensation feature.
|
SpringbackCompensationBuilder
Used to create or edit a
SpringbackCompensation feature. |
SpringbackCompensationBuilder.DefinedByType
The type of input data that defines the compensation.
|
SpringbackCompensationBuilder.DegreeType
The polynomial degree type.
|
SpringbackCompensationBuilder.ResultSheetType
The type of sheet body you would like created as output.
|
SteelInsertBuilder
Represents a Steel Insert feature builder.
|
SteelInsertBuilder.HoleGridOrientationData
This class holds the data returned from
SteelInsertBuilder.getHoleGridOrientation() |
SteelInsertBuilder.InsertTypeOption
Settings for the insert type.
|
SteelInsertBuilder.MainProfileData
This class holds the data returned from
SteelInsertBuilder.getMainProfile() |
SteelInsertSectionBuilder
Represents a Steel Insert Section sub feature.
|
SteelInsertSectionBuilder.ExtensionTypeOption
Settings for the extension type.
|
SteelInsertSectionBuilder.FormingAttributesData
This class holds the data returned from
SteelInsertSectionBuilder.getFormingAttributes() |
SteelInsertSegmentChildBuilder
Represents a Steel Insert Segment Child sub feature.
|
SteelInsertSegmentChildBuilder.ExtensionTypeOption
Settings for the extension type.
|
SteelInsertSegmentChildBuilder.InsertTypeOption
Settings for the insert type.
|
SteelInsertSegmentParentBuilder
Represents a Steel Insert Segment Parent sub feature.
|
SteelInsertSegmentParentBuilder.ExtensionTypeOption
Settings for the extension type.
|
SteelInsertSegmentParentBuilder.InsertTypeOption
Settings for the insert type.
|
ThroatChildBuilder
Represents a Die Throat Child sub feature.
|
ThroatChildBuilder.ExtensionAttributesData
This class holds the data returned from
ThroatChildBuilder.getExtensionAttributes() |
ThroatChildBuilder.TypeOption
Settings for the type of the throat section.
|
ThroatParentBuilder
Represents a Die Throat Parent sub feature.
|
ThroatParentBuilder.ExtensionAttributesData
This class holds the data returned from
ThroatParentBuilder.getExtensionAttributes() |
ThroatParentBuilder.TypeOption
Settings for the type of the throat section.
|
Tip.MapEdgeData
This class holds the data returned from
Tip.mapEdge(nxopen.IProfile) |
TrimFlangeDieAssistantBuilder
Represents a
TrimFlangeDieAssistantBuilder
To create a new instance of this class, use DieCollection.trimFlangeDieAssistant(nxopen.features.Feature) Created in NX5.0.0 |
TrimLineDevelopmentBuilder
Represents a
TrimLineDevelopment builder
To create a new instance of this class, use DieCollection.createTrimLineDevelopmentBuilder(nxopen.features.Feature) Created in NX6.0.0 |
TrimLineDevelopmentBuilder.Convergency
The solver convergency level of onestep unform.
|
TrimLineDevelopmentBuilder.MaterialTypeName
Indicates type of material
|
TrimLineDevelopmentBuilder.MeshElement
The 2-D mesh element type of onestep unform.
|
TrimLineDevelopmentBuilder.OutputMethodName
Indicates which trim curves to output
|
TrimLineDevelopmentBuilder.SmoothingName
Indicates type of curve smoothing
|
TrimLineDevelopmentBuilder.Surface
The surface types of onestep unform.
|
TrimTaskBuilder
Represents a Trim Task feature builder.
|
TrimTaskBuilder.CameraLayerAndXmlpData
This class holds the data returned from
TrimTaskBuilder.getCameraLayerAndXmlp() |
TrimTaskBuilder.CamTypes
Settings for the cam type of the trim task.
|
TrimTaskBuilder.CheckAndMovePlanesData
This class holds the data returned from
TrimTaskBuilder.checkAndMovePlanes(nxopen.features.Feature, nxopen.features.Feature, nxopen.ISurface, nxopen.ISurface) |
TrimTaskBuilder.MatchCutTypes
Settings for the match cut type of the trim task.
|
TrimTaskBuilder.TrimBoundsData
This class holds the data returned from
TrimTaskBuilder.getTrimBounds() |
UncutRegionsBuilder
Calculates the uncut regions of a curve given a radius value for the cut tool.
|
UncutRegionsBuilder.ResultsType
Indicates which side of curve to check
|
WearPlateLocChildBuilder
Represents a Die Wear Plate Locator sub feature.
|
WearPlateLocChildBuilder.PadAttributesData
This class holds the data returned from
WearPlateLocChildBuilder.getPadAttributes() |
WearPlateLocChildBuilder.PositionType
Settings for the positioning of the locator relative to the wear plate.
|
WearPlateLocParentBuilder
Represents a Die Wear Plate Locator sub feature.
|
WearPlateLocParentBuilder.PadAttributesData
This class holds the data returned from
WearPlateLocParentBuilder.getPadAttributes() |
WearPlateLocParentBuilder.PositionType
Settings for the positioning of the locator relative to the wear plate.
|
Class and Description |
---|
DieCollection
Represents a Die Engineering/Design feature builder.
|
DieLimitsBuilder
Limits a path to a segment of the path.
|
Class and Description |
---|
DieLimitsBuilder
Limits a path to a segment of the path.
|
DieLimitsBuilderList
Represents a list of objects.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.