Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.BASIC
Section consists of all segments in a step like shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.BLANK
No section shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.BLEND
Section consists of a single radius type segment to define the blend shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.CHANNEL
Section consists of all segments in a channel shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.DRAW_BAR
Section consists of all segments in a draw bar shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.EXTENSION
Section consists of a plus segment only.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.REUSE
Section shape is read from reuse library.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.SIMPLE
Section consists of trim ledge, punch radius, and second stretch wall segments.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.SYSTEM
Section shape determined by blending neighboring sections.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.USER_DEFINED
Section shape is user defined.
|
Modifier and Type | Method and Description |
---|---|
AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.sectionShape()
Returns the section shape.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SectionShapeType |
AddendumSectionBuilder.SectionShapeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SectionShapeType[] |
AddendumSectionBuilder.SectionShapeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddendumSectionBuilder.setSectionShape(AddendumSectionBuilder.SectionShapeType sectionShape)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.