public static class AddendumSectionBuilder.SectionShapeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BASIC
Section consists of all segments in a step like shape.
|
static int |
_BLANK
No section shape.
|
static int |
_BLEND
Section consists of a single radius type segment to define the blend shape.
|
static int |
_CHANNEL
Section consists of all segments in a channel shape.
|
static int |
_DRAW_BAR
Section consists of all segments in a draw bar shape.
|
static int |
_EXTENSION
Section consists of a plus segment only.
|
static int |
_REUSE
Section shape is read from reuse library.
|
static int |
_SIMPLE
Section consists of trim ledge, punch radius, and second stretch wall segments.
|
static int |
_SYSTEM
Section shape determined by blending neighboring sections.
|
static int |
_USER_DEFINED
Section shape is user defined.
|
static AddendumSectionBuilder.SectionShapeType |
BASIC
Section consists of all segments in a step like shape.
|
static AddendumSectionBuilder.SectionShapeType |
BLANK
No section shape.
|
static AddendumSectionBuilder.SectionShapeType |
BLEND
Section consists of a single radius type segment to define the blend shape.
|
static AddendumSectionBuilder.SectionShapeType |
CHANNEL
Section consists of all segments in a channel shape.
|
static AddendumSectionBuilder.SectionShapeType |
DRAW_BAR
Section consists of all segments in a draw bar shape.
|
static AddendumSectionBuilder.SectionShapeType |
EXTENSION
Section consists of a plus segment only.
|
static AddendumSectionBuilder.SectionShapeType |
REUSE
Section shape is read from reuse library.
|
static AddendumSectionBuilder.SectionShapeType |
SIMPLE
Section consists of trim ledge, punch radius, and second stretch wall segments.
|
static AddendumSectionBuilder.SectionShapeType |
SYSTEM
Section shape determined by blending neighboring sections.
|
static AddendumSectionBuilder.SectionShapeType |
USER_DEFINED
Section shape is user defined.
|
Modifier and Type | Method and Description |
---|---|
static AddendumSectionBuilder.SectionShapeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SectionShapeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SectionShapeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AddendumSectionBuilder.SectionShapeType BASIC
public static final AddendumSectionBuilder.SectionShapeType DRAW_BAR
public static final AddendumSectionBuilder.SectionShapeType SIMPLE
public static final AddendumSectionBuilder.SectionShapeType CHANNEL
public static final AddendumSectionBuilder.SectionShapeType BLEND
public static final AddendumSectionBuilder.SectionShapeType EXTENSION
public static final AddendumSectionBuilder.SectionShapeType SYSTEM
public static final AddendumSectionBuilder.SectionShapeType USER_DEFINED
public static final AddendumSectionBuilder.SectionShapeType REUSE
public static final AddendumSectionBuilder.SectionShapeType BLANK
public static final int _BASIC
public static final int _DRAW_BAR
public static final int _SIMPLE
public static final int _CHANNEL
public static final int _BLEND
public static final int _EXTENSION
public static final int _SYSTEM
public static final int _USER_DEFINED
public static final int _REUSE
public static final int _BLANK
public static AddendumSectionBuilder.SectionShapeType valueOf(int value)
public static AddendumSectionBuilder.SectionShapeType valueOf(String name)
public static AddendumSectionBuilder.SectionShapeType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.