Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.FIVE
Degree is 5
|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.SEVEN
Degree is 7
|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.THREE
Degree is 3
|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.TWO
Degree is 2
|
Modifier and Type | Method and Description |
---|---|
SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.degree()
Returns the polynomial degree (one unit less than the order).
|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpringbackCompensationBuilder.DegreeType |
SpringbackCompensationBuilder.DegreeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpringbackCompensationBuilder.DegreeType[] |
SpringbackCompensationBuilder.DegreeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpringbackCompensationBuilder.setDegree(SpringbackCompensationBuilder.DegreeType degree)
License requirements: die_engineering ("DIE ENGINEERING") OR nx_freeform_2 ("advanced freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.