Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.OutputMethodName.BOTH
Both geometric and corrected curves
|
static TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.OutputMethodName.CORRECTED
Corrected curve only
|
static TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.OutputMethodName.GEOMETRIC
Geometric curve only
|
Modifier and Type | Method and Description |
---|---|
TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.outputMethod()
Returns the curve output method - geometric, corrected or both
License requirements: None. |
static TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.OutputMethodName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.OutputMethodName |
TrimLineDevelopmentBuilder.OutputMethodName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.OutputMethodName[] |
TrimLineDevelopmentBuilder.OutputMethodName.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimLineDevelopmentBuilder.setOutputMethod(TrimLineDevelopmentBuilder.OutputMethodName outputMethod)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.