Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.BLANK
No orientation.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.CONJUGATE
Use conjugate orientation.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.DEFAULT
Orient perpendicular to tangency curve.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.INCIDENT_EDGE
Orient from incident edge.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.ISOPARAMETRIC
Orient along isoparametric line of closest face.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.THREE_DPERPENDICULAR
Orient 3D perpendicular to tangency curve
|
Modifier and Type | Method and Description |
---|---|
AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.sectionOrientation()
Returns the section orientation.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddendumSectionBuilder.SectionOrientationType |
AddendumSectionBuilder.SectionOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddendumSectionBuilder.SectionOrientationType[] |
AddendumSectionBuilder.SectionOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddendumSectionBuilder.setSectionOrientation(AddendumSectionBuilder.SectionOrientationType sectionOrientation)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.