Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadSegmentBuilder |
DrawBeadBuilder.createDrawBeadSegment()
Creates a
DrawBeadSegmentBuilder builder. |
DrawBeadSegmentBuilder |
DrawBeadSegmentBuilderList.findItem(int index)
Returns the object at the input index.
|
DrawBeadSegmentBuilder[] |
DrawBeadSegmentBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadSegmentBuilderList.append(DrawBeadSegmentBuilder object)
Appends an object to the list
License requirements: None. |
void |
DrawBeadSegmentBuilderList.append(DrawBeadSegmentBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DrawBeadSegmentBuilderList.erase(DrawBeadSegmentBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DrawBeadSegmentBuilderList.erase(DrawBeadSegmentBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DrawBeadSegmentBuilderList.findIndex(DrawBeadSegmentBuilder obj)
Finds the index where the input object appears.
|
void |
DrawBeadSegmentBuilderList.insert(int location,
DrawBeadSegmentBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DrawBeadSegmentBuilderList.setContents(DrawBeadSegmentBuilder[] objects)
Sets the contents of the entire list.
|
void |
DrawBeadSegmentBuilderList.swap(DrawBeadSegmentBuilder object1,
DrawBeadSegmentBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.