Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DieDirectionBuilder.DirectionType |
DieDirectionBuilder.DirectionType.COORDINATE_SYSTEM
Define a coordinate system (-Z) for the direction.
|
static DieDirectionBuilder.DirectionType |
DieDirectionBuilder.DirectionType.SELECTION
Select a coordinate system (-Z) or plane for the direction.
|
static DieDirectionBuilder.DirectionType |
DieDirectionBuilder.DirectionType.VECTOR
Define a vector for the direction.
|
Modifier and Type | Method and Description |
---|---|
DieDirectionBuilder.DirectionType |
DieDirectionBuilder.inputType()
Returns the type of input that defined the direction
License requirements: None. |
static DieDirectionBuilder.DirectionType |
DieDirectionBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieDirectionBuilder.DirectionType |
DieDirectionBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieDirectionBuilder.DirectionType[] |
DieDirectionBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DieDirectionBuilder.setInputType(DieDirectionBuilder.DirectionType inputType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.