Package | Description |
---|---|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
Modifier and Type | Field and Description |
---|---|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.MALE
Creates the male bead only.
|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.NONE
Creates a small sphere on the centerline.
|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.PLUS_FEMALE
Creates the male and female bead.
|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.PLUS_SHEET_METAL
Creates the male, female and sheet metal bead.
|
Modifier and Type | Method and Description |
---|---|
DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.output()
Returns the output to be constructed by the draw bead feature.
|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.OutputTypes |
DrawBeadBuilder.OutputTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.OutputTypes[] |
DrawBeadBuilder.OutputTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DrawBeadBuilder.setOutput(DrawBeadBuilder.OutputTypes output)
License requirements: die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.